What does being economical have to do with good journalism?

Even an acclaimed radio station must economize, except when it comes to programming. So, Radio Bremen uses Siemens Building tech to save money, investing in great journalism instead.
Building Management

On Air 24/7 - reliable and energy efficient

Radio Bremen depends on building technology from Siemens to make sure their broadcast signal is 100 percent trouble free, which is exactly what listeners and viewers expect. Innovative energy data management enables the station to optimize its energy efficiency continuously.

Always quickly and reliably informed

Television, radio and internet keep people up to date, every minute, every second. Punctuality and reliable broadcast transmission are top priority. Radio Bremen is ideally equipped to provide its listeners and viewers around the clock information and entertainment from its broadcasting center, comprised of three new buildings equipped with innovative building tech that offers one hundred percent operational availability.

 

Siemens modular Desigo building platform seamlessly connects the buildings with an environmentally friendly air-conditioning and ventilation system creating one efficient overall system. The building automation concept includes several thousand data points that are operated via Desigo. This also enables equipment from different manufacturers to be integrated into the system. Innovative building technologies on site include condensing boilers and chillers, and alternative energy sources such as underground well cooling systems, concrete core cooling and heat recovery. The system is very stable, thanks to modern remote maintenance technology.

 

Another advantage of this solution is energy data management supported by the cloud-based Navigator powered by Sinalytics™. With the Navigator, Radio Bremen can easily review consumption data, evaluating and identifying savings potential as a result. This allows the radio network to continually optimize its properties, cutting energy costs and maximizing energy efficiency.

Our technology must always function. If the cooling system or the power fails, we are off the air.

Werner Thomas, Manager of Building Services Technology, Radio Bremen

Infographic

Optimized for perfect broadcast operations

Radio and TV broadcasters deliver news, opinion, and in-depth stories everyday. In Radio Bremen's broadcast center, innovative building technology lets the editorial team and show hosts always keep a clear head on the air, even when playing the hottest music or reporting on controversial topics.

One hundred percent operations availability. Round the clock.
Innovative and Energy efficient.

  • Combine new and existing technology in one complete system.
  • Latest remote maintenance
    technology for failsafe performance
  • Navigator powered by Sinalytics:to evaluate consumption data
    and identify savings potential
Building Automation
Building Control
Energy Data Management
Remote Access and Monitoring
Heating and Cooling System
Fire Alarm System
Intrusion Detection System
Service and Maintenance

Modern building technology can achieve up to a

20%

reduction in gas consumption

within one year

Portfolio

Reliable systems for efficient buildings

Siemens Building technologies integrates new and existing infrastructures into a complete unified system. The solutions offer reliable control of the entire infrastructure and ensure efficient use of energy and reliable fire protection.

For more information please send us a message.

First name is required.
Last name is required.
E-mail is required. E-mail has to be of format 'text@text.text'.
Company/Organisation is required.
Your Message is required.
* Required
Cancel

Your request has been successfully processed.

Thank you for your contribution.

Your message could not be sent due to a technical error.

Please excuse the inconvenience. In case the problem persists, please try again at a later time.