More energy with the same amount of fuel

    Maximizing energy generation during the harvest and off-season, in sugar and alcohol plants, it is possible: with state-of-the-art technology and regenerative cycle.    
Energy generation from biomass

The largest turbine in Brazil's sugar and alcohol industry

Sugar and ethanol plants generate energy from sugarcane bagasse or straw for many years. Recently, new technologies in steam turbines are drastically improving this activity and increasing its profitability.

Energy galore

The Delta Sucroenergia Group, which operates three plants in the state of Minas Gerais (Brazil), needed to modernize its energy generation process and, for that, it sought for solutions in the market. Operating in the area of ​​sugar and ethanol production, the company intended to increase the energy generated from the biomass derived from sugarcane, guaranteeing energy for own consumption, besides marketing the surplus to the National Interconnected System, increasing the company's revenue.

The company realized that as important as receiving proposals for the implementation of new solutions, are the need and benefits of having a previous analysis of the thermodynamic mass and energy balance. Focus: Ensure the reliability and performance of the equipment, to achieve the customer's goals. The prospect was designed not only to replace existing equipment at the plant - two turbines that generated 15 MW of power each - and to increase generation capacity, through a larger and more efficient turbine.

The response to the Delta Plant challenge was the SST600 steam turbine, a model with recognized performance in Brazil and worldwide, making the project a pioneer case in two important aspects. The first of them: The turbine of the Delta Plant is the first in the sector directly coupled to the generator, delivering increased operational safety and greater energy efficiency. The second: An innovative layout for the installation of the set, in an external environment, reducing the expenses with civil works significantly.

The new turbine will allow the Delta Plant to generate more than 376 MWh per year, which would be enough to supply a city such as São Bernardo do Campo. The city of São Bernardo do Campo has 740,000 inhabitants and is located in the metropolitan region of São Paulo, the largest city in Brazil.

It is also the largest turbine in the sugar and alcohol sector in Brazil. With a power of 73.5 MW, the plant not only fully meets the demand for internal processes, but exports around 56MW to the external grid.

With the high technological level of the turbine, the Delta Sucroenergia Group guaranteed a strong reduction of costs in the long term, since the equipment would not require maintenance for a period of at least five years.

Siemens is a highly qualified company in power generation. Its turbine, in addition to generating more energy with the same amount of steam, has internationally proven know-how. So I was happy that the equipment was signed and manufactured by Siemens
Roberto Lyra, President of the Delta Sucroenergia Group


Infographic

Delta Plant

New structure guarantees more generation and energy capacity.

Power generated

Before

20

MWh

After

68

MWh
Power exported

Before

6

MWh

After

50

MWh

Growth of0%

Steam Turbine SST600
Turn on the turbine
Drag the button to the other side

Internal consumption + energy exportation

Equivalent to the consumption of a city like São Bernardo do Campo (state of SP, Brazil), with 740 thousand inhabitants

0,0

=

São Bernardo do Campo

Siemens SST-600: Highly versatile

Technological level upper attention to detail

Drag and view the SST-600 turbine in detail

Innovative technology

Direct drive equipment

Direct drive

Increased investment in the turbine
Generator with higher investment
Lower maintenance (OpEX cost)

Direct drive

Drive with reducer

Reduced turbine price
Generator with lower investment
Higher maintenance (OpEX cost)

Drive with reducer

Turbine Portfolio

Conventional energies

Although the generation of electric energy can be made by several sources, usually a rotating equipment is responsible for driving an electric generator. Siemens has in its product line rotary equipment for these drives.