In this module, the reader is acquainted with the essential functions of the LOGO! logic module 12/24RC with a communication module to the AS interface.
In this module, the reader learns how to program and parameterize the WinAC soft-PLC. This puts the PROFIBUS DP into service with WinAC as master and the ET 200L as slave.
In this module, the reader learns how the PROFIBUS DP is commissioned with an S7-300 with the CPU-342-5 DP communication processor as master and the ET 200L as slave.
In this module, the reader learns how the PROFIBUS DP is commissioned with one S7-300 with the CPU-342-5 DP communication processor as master and another as the slave.
In this module, the reader learns how an FDL connection on the PROFIBUS DP is commissioned with two S7-300s with the CPU-342-5 DP communication processor as master.
In this module, the reader learns how a safety-related application on the AS-interface (ASIsafe) is commissioned. This uses the safety monitor device at the AS interface.
In this module, the reader learns how a safety-related application on PROFIBUS (PROFIsafe) is commissioned. In this case, the CPU 315F-2 PN/DP is used on the PROFIBUS as master with an ET 200S as slave.
In this module, the reader learns how a safety-related application on PROFIBUS (PROFIsafe) is commissioned. In this case, the CPU 315F-2 DP is used on the PROFIBUS as master with an ET 200S F-CPU as slave.
In this module, the reader learns how the PROFIBUS DP is commissioned with an S7-300 with the CPU 342-5DP communication processor as master and the ET 200S as slave.