TIA Portal Modules | from V13
100 Special Modules
Below you will find special modules of the TIA Portal learn-/training documents. These modules address overarching topics, e.g.:
• Vision
• Siwarex
• Web servers
• Security
• Safety
• Energy efficiency
• Extended communication
• RFID
The following pages show how an RF210R IO-Link RFID sensor can be put into operation on an IO-Link module in a project with SIMATIC S7-1500 and ET 200SP and how data can be written and read to mobile data media using the blocks from the "IOL_READ_WRITE_DATA_LIB_V3.1" library. Read and write operations are performed via a visualization on a SIMATIC TP700 Comfort panel, which must also be created.