Technical Papers and Webinars

Are you interested in the latest technical developments in power generation?

Find and download the latest technical papers and presentations of industry experts who share their know-how on current trends and projects. This month's special is our white paper “Evolutionary development of Siemens SGT-800 – A ground for reliable upgrades”. The SGT-800 has developed continuously during the last 20 years with an initial rating of 43MW. During this time frame seven upratings have been released – with an average output increase of 2MW with each new rating and a related efficiency increase – where each step taken is based in the operational experience gained from previous generations and adding the latest technologies and materials. 

Download

Explore our latest papers and webinars

Presented at POWER-GEN Asia 2018

Reheat solutions significantly increase the overall efficiency of a biomass plant and are therefore an optimal solution to produce more energy without having to use more fuel. Siemens offers single-casing reheat solutions up to 65 MW and dual-casing reheat solutions for higher steam temperatures and highest efficiency solution. A standardized package of highest efficiency solution steam turbines that follow the design philosophy Enhanced Platform offers an economical solution for biomass applications. This fixed design enables short manufacturing periods, fast ex-works delivery and makes these turbines much more cost-effective.

Presented at POWER-GEN Asia 2018

Steam power plants will continue to be the backbone for reliable, affordable and sustainable power for fast developing economies. The new steam power plants follow the requirements for highest efficiency and flexibility in order to incorporate the flexible Steam Power Plants into the forecasted energy mix with renewable power and have the best economics over the life cycle. By upgrading the SST-5000 Steam Turbine for 300MW steam power plants, Siemens provides highest efficiency for ultra-super critical plants with small power output. The combination of the latest technology with digital applications explained in this paper optimizes the operation for the owner with HELEBE – Highest Efficiencies, Lowest Emissions and Best Economics.
 

Presented at Sugar Industry 2017

Cane sugar is manufactured in sugar mills in tropical and semi-tropical regions. For every 10 t of sugarcane crushed, a sugar factory produces nearly 3 t of bagasse as a byproduct. The bagasse contains enough energy to allow the mill to be self-sufficient with respect to steam and power requirements. Depending on the mill’s efficiency, location, and the local electricity grid, excess power may also be fed into the grid for additional revenue. 

In a typical cane sugar mill, approximately 500 kg of low-pressure process steam are required to process 1 t of cane. Along with generating steam for the process, steam turbines are also used to drive the cane milling tandems. Condensing or backpressure turbines in a single or multistage design can be used in the sugar-making process. Optionally, the turbines can also be equipped with single extraction options or multiple controlled (pass-out) and uncontrolled (bleeding) extraction options. Single-stage back-pressure impulse-type turbines have about 25% to 30% efficiency. A condensing steam turbine (multi-stage steam turbines) can operate at efficiencies from 80% to 89%.

The condensation path maximizes electrical power output. The low-pressure steam required for the sugar/ethanol manufacturing process can be extracted from the appropriate stage of a condensing turbine. If the factory has excess steam due to appropriate energy-saving equipment, the energy contained in the steam can be recovered as electricity using a condensing turbine.

Presented in Thermal Engineering Russia 2017

Siemens Enhanced Platform is a technological platform allowing the development of steam-turbine units with a power output up to 250 MWel. It uses standardized turbine elements, such as bearings, casings or steam admission components, for example, with the best innovative design features and proven in operation for assembling various types of customized turbines. The system makes it possible to enhance turbine standardization, decrease production cost, and cut lead time. Siemens Enhanced Platform designs feature higher efficiency, improved reliability, better flexibility, and longer overhaul intervals. Additionally, turbine units delivered as fully shop-assembled items can be installed onto a foundation without using bridge cranes in the turbine hall. 

Presented at POWER-GEN Asia Thailand 2016

Power generation fired on carbon-based fuels places high priority not only on profitability, but also on responsible fuel handling and consumption. Efforts to reduce CO2 emissions undertaken in the past have focused on large, state-of-the-art steam power plants in the higher output classes. Download the technical paper available and learn more about the measures developed to increase efficiency and flexibility for large units.

The Organisation for Economic Co-operation and Development (OECD) recently addressed the environmental requirements as a precondition for export financing for the entire range of coal-fired power plants. Going forward, the good experiences gained from existing high-end ultra-super critical (USC) coal-fired power plants needs to be transferred to power plants of the 350-MW size. Innovative products are needed to serve this market segment in the most beneficial way for power plant owners.

Siemens has modified its core components to address these new requirements. Siemens steam turbines demonstrate how technology for (U)SC applications in larger units has been introduced in proven turbine designs for subcritical applications. For steam turbine generators, Siemens offers an innovative mix of proven components and technologies to reduce initial, operational and service costs and provide top performance with operational flexibility.

Presented at POWER-GEN International 2018

The technical paper available for download provides valuable details and insights into the evolutionary Siemens HL-class gas turbines and power plants. The HL-class combines best-in-class technology innovations with the rich heritage of Siemens proven SGT-8000H series design resulting in a Technology carrier to the next level of performance. The HL-class is designed for highest operational reliability and flexibility to fulfill the requirements of base load units while also being a perfect fit for peaker applications.

Focus of the webinar is the SGT-A45 with which Siemens has developed the next generation in aeroderivative gas turbine technology. The SGT-A45 provides immediate and reliable power and has been optimized for easy transportation and installation to deliver more power and higher efficiency than any other mobile gas turbine in the world.

Focus of the webinar are the SGT-9000HL engines for the 50Hz and 60Hz markets. The HL-class is designed for highest operational reliability and flexibility to fulfill the requirements of base load units while also being a perfect fit for flexible applications. This makes the HL-class turbines a versatile solution for operators who anticipate energy systems with a rapidly increasing share of fluctuating production by renewables. 

White Paper


This white paper available for download provides insights into Siemens philosophy of continuously developing the SGT-800 to cope with changing market requirements. The SGT-800 has developed continuously during the last 20 years with an initial rating of 43MW. During this time frame seven upratings have been released – with an average output increase of 2MW with each new rating and a related efficiency increase – where each step taken is based in the operational experience gained from previous generations and adding the latest technologies and materials.   

Presented at POWER-GEN Africa 2017

In Africa, diesel or heavy fuel oil (HFO) are traditionally used as the primary fuel or back-up fuel for fossil-fueled power generation plants at all scales. In comparison, Propane offers a potentially cleaner and more cost-effective alternative. The technical paper and presentation available for download compare the economic, operational and environmental benefits of using propane as a fuel for gas turbine-based power generation. 

Presented at Electrify Europe 2018



The technical paper and presentation available for download examine the potential to use a wide range of unconventional low carbon fuels, hydrogen and ammonia in gas turbines, and reviews operational experience gained in various industries and the future potential developments for further decarbonization of power generation.

Presented at POWER-GEN Asia 2017

The power generation industry has a major role to play in reducing global greenhouse gas emissions, and carbon dioxide (CO2) in particular. The technical paper and presentation available for download examine the potential use of unconventional low carbon fuels and hydrogen in industrial gas turbines. Additionally, the authors review the operational experience gained in various industries and give an outlook for potential further decarbonization of power generation in the future.

Presented at POWER-GEN Europe 2017

The technical paper and presentation available for download provide a detailed description of the test setup and evaluation of the operational data for a single burner SGT-750 combustion system in the atmospheric combustion test rig for the gas blends at cold ambient conditions.    

Presented at POWER-GEN Asia 2017

The technical paper and presentation available for download give an overview of the new SGT-A45 Siemens mobile gas turbine unit that was recently developed for a rapidly growing market. This product achieves unsurpassed levels of power density with the typical attributes of mobile units: installation in two weeks or less, and a high degree of mobility to facilitate initial delivery or relocation of the unit by road, sea or air. It features an aero-derivative engine core that utilizes proven components and thus inherits best-in-class levels of fuel efficiency and operational flexibility.

The gas turbine and its auxiliary systems are packaged onto three trailers, in a configuration carefully optimized to facilitate transportation, minimize interconnections between different trailers and simplify the installation on site. With the majority of commissioning activities completed at the factory, duration, cost and uncertainty of site installation are greatly reduced. 

Presented at POWER-GEN Europe 2017

The technical paper and presentation available for download give a detailled report of the latest achievements in Siemens' ongoing development to allow for higher hydrogen shares in co-firing gas turbines. The aim is to reach hydrogen contents in natural gas of higher than 40 vol% in the 3rd and 4th generation dry low emission (DLE) combustion systems. Additive manufacturing, 3D printing, is used for rapid prototyping of burner hardware. 

Presented at POWER-GEN Europe 2017

The technical paper and presentation available for download highlight successful projects using Siemens SGT-8000H gas turbine technology. The documents also give an outlook for the SGT-8000H series based on its proven capabilities: With low life cycle costs, high reliability and availability, operational flexibility, and low emissions, the SGT-8000H series sets the trend for clean fossil power generation worldwide. 

Presented at POWER-GEN Europe 2016

New technologies are quickly and effectively validated at Siemens' own test centers and on customer sites worldwide. This paper describes the features and technical details of the various Siemens’ own test facilities and the derivable benefits for the power plant operators.

Presented at VGB Fachtagung "Gasturbinen und Gasturbinen-Betrieb" Germany 2017

This technical paper explains the enhanced demands on gas turbines due to changing market requirements. Gas turbines need to be cold and fast restarted. Adaptations in the modes of operation can contribute to life time extension of various power plant components, such as the gas turbine and the HRSG. 


Presented at POWER-GEN Asia 2018

Continuously growing renewables share has a significant impact on the synchronous power production equipment and also on the transmission system operation. The synchronous generators are simple and reliable grid stabilizers with unique capabilities. The extended contribution to grid stability can be achieved by different configurations of synchronous condensers with fly wheels, back-up drives and optionally combined with storage equipment.

Presented at POWER-GEN International 2016

The technical paper available for download introduces the new pressurized air-cooled generator SGen-2000P series and explains its design features and components, its benefits and its serviceability. 

Presented at POWER-GEN Asia 2018 


Mobility, flexibility and no need for land acquisition are the most prominent features which distinguish SeaFloat power plants from conventional land-based plants. These features come along with short lead time due to high prefabrication grade and enhanced plug & play concept as well as reduced overall project investments making them interesting for various applications. Siemens SeaFloat applications are currently based on, but not limited to the on the gas turbine frames SGT-A65, SGT-800 and SGT-8000H series. This paper describes the SeaFloat Power Plant concept, which comprises the complete SeaFloat Power Plant solution for power supply to the grid.

Presented at POWER-GEN Asia 2018 (Best Paper Award within the category ‘Power Plant Technologies’)

The clear benefit of a water-free combined cycle power plant solution is the ability to offer ‘zero water’ flexible distributed power generation with combined cycle efficiencies in regions where water is unavailable or a scarce resource, without incurring large additional costs or seeing significant reductions in power plant performance. Implementing the Organic Rankine Cycle (ORC) offers a competitive alternative to conventional ‘steam’ combined cycle concepts.

Presented at POWER-GEN Asia 2018

Reheat solutions significantly increase the overall efficiency of a biomass plant and are therefore an optimal solution to produce more energy without having to use more fuel. Siemens offers single-casing reheat solutions up to 65 MW and dual-casing reheat solutions for higher steam temperatures and highest efficiency solution. A standardized package of highest efficiency solution steam turbines that follow the design philosophy Enhanced Platform offers an economical solution for biomass applications. This fixed design enables short manufacturing periods, fast ex-works delivery and makes these turbines much more cost-effective.

Presented at POWER-GEN Africa 2018

The technical paper and presentation available for download focus on solutions available especially for the generation of Fast Mobile Power for sub-Sahara Africa which remains the leading region in the world where rapid development is primarily restricted by access to electricity. The authors discuss the role auf Aeroderivative powered mobile generators supporting the infrastructure development.

Since operational safety and reliability are major important requirements in the power generation business and its production systems are highly complex, digitalization has already been introduced since computers were available. However continuous progress is being made and increasing use of data during manufacturing and operation increase customer value.

This paper describes digital applications along the end2end value chain of power plants with a special focus on steam turbines and steam power plants. Big data based probabilistic methods are used during the design of components. Industry 4.0 focused on manufacturing processes adds major benefit to product quality (e.g. by closed-loop chain of computer aided design and manufacturing). Artificial intelligence of control systems considerably improves operational performance by connection of power plant components and self-learning optimization algorithms. Finally big data analysis of operating records in combination with the digital twin of the plant enables condition based maintenance and adds value for customers to optimize inspections.

Presented at VGB Fachtagung "Gasturbinen und Gasturbinen-Betrieb" Germany 2017

This technical paper presents the case study Bayonne Energy Center, a successful plant for grid support in a weather driven, highly volatile grid due to fast start and operational flexibility, high full and part load efficiency and high reliability and availability.

Presented at POWER-GEN Africa 2017

The technical paper and presentation available for download show how operational flexibility can be provided by small light industrial and aero-derivative gas turbines and their characteristics: fast response times via fast ramp rates, high availability and low maintenance downtimes due to the core-swap capability of specific gas turbine designs. The authors discuss specific market and customer challenges, explaining concepts and specific project solutions.

Presented at POWER-GEN Asia Thailand 2016

Power generation fired on carbon-based fuels places high priority not only on profitability, but also on responsible fuel handling and consumption. Efforts to reduce CO2 emissions undertaken in the past have focused on large, state-of-the-art steam power plants in the higher output classes. Download the technical paper available and learn more about the measures developed to increase efficiency and flexibility for large units.

The Organisation for Economic Co-operation and Development (OECD) recently addressed the environmental requirements as a precondition for export financing for the entire range of coal-fired power plants. Going forward, the good experiences gained from existing high-end ultra-super critical (USC) coal-fired power plants needs to be transferred to power plants of the 350-MW size. Innovative products are needed to serve this market segment in the most beneficial way for power plant owners.

Siemens has modified its core components to address these new requirements. Siemens steam turbines demonstrate how technology for (U)SC applications in larger units has been introduced in proven turbine designs for subcritical applications. For steam turbine generators, Siemens offers an innovative mix of proven components and technologies to reduce initial, operational and service costs and provide top performance with operational flexibility.

Presented at Sugar Industry 2017

Cane sugar is manufactured in sugar mills in tropical and semi-tropical regions. For every 10 t of sugarcane crushed, a sugar factory produces nearly 3 t of bagasse as a byproduct. The bagasse contains enough energy to allow the mill to be self-sufficient with respect to steam and power requirements. Depending on the mill’s efficiency, location, and the local electricity grid, excess power may also be fed into the grid for additional revenue.

In a typical cane sugar mill, approximately 500 kg of low-pressure process steam are required to process 1 t of cane. Along with generating steam for the process, steam turbines are also used to drive the cane milling tandems. Condensing or backpressure turbines in a single or multistage design can be used in the sugar-making process. Optionally, the turbines can also be equipped with single extraction options or multiple controlled (pass-out) and uncontrolled (bleeding) extraction options. Single-stage back-pressure impulse-type turbines have about 25% to 30% efficiency. A condensing steam turbine (multi-stage steam turbines) can operate at efficiencies from 80% to 89%. 

Presented at POWER-GEN Asia 2018

Reheat solutions significantly increase the overall efficiency of a biomass plant and are therefore an optimal solution to produce more energy without having to use more fuel. Siemens offers single-casing reheat solutions up to 65 MW and dual-casing reheat solutions for higher steam temperatures and highest efficiency solution. A standardized package of highest efficiency solution steam turbines that follow the design philosophy Enhanced Platform offers an economical solution for biomass applications. This fixed design enables short manufacturing periods, fast ex-works delivery and makes these turbines much more cost-effective.

Presented at POWER-GEN Asia 2018

Integrated Solar Combined Cycle Power Plants (ISCCs), comprising a Concentrated Solar Power plant and a natural gas fired combined cycle plant, have the potential to simultaneously reduce fossil fuel consumption, provide secure, highly predictable electricity generation, and reduce the cost of integrating renewable energy into a power system. This paper evaluates whether replacing the steam bottoming cycle with an Organic Rankine Cycle (ORC) alternative can provide a simpler, lower cost distributed ISCC solution that can be utilised on smaller and island grid systems, or mini- and micro-grids, to provide an affordable, water-free low carbon power generation system.

Presented at POWER-GEN Asia 2017

Large scale deployment of intermittent renewable power generation is creating increasing technical and economic challenges for system operators, power generators and investors. System stability is compromised as inverter-connected wind turbines and photovoltaics do not provide the rotational system conventionally used to maintain grid frequency. The technical paper available for download describes different solutions to enhance the operator's flexibility, such as integrating a Solar Combined Cycle Power Plant. 

Presented at VDI International Conference 2017

The technical paper available for download highlights global trends influencing the energy markets and presents answers to these challenges by customizing flexible offers with positive commercial outcomes. Examples are hydrogen co-firing in Siemens gas turbines, SIESTART hybrid solutions, mobile and fast power supply, among others. 

Presented at POWER-GEN International 2017

Large scale deployment of intermittent renewable power generation is creating increasing technical and economic challenges for system operators, power generators and investors. System stability is compromised as inverter-connected wind turbines and photovoltaics do not provide the rotational system conventionally used to maintain grid frequency. The technical paper available for download describes different solutions to enhance the operator's flexibility, such as integrating a Solar Combined Cycle Power Plant, for example.

Presented at POWER-GEN Africa 2016

The technical paper available for download focuses on the Siemens gas turbine portfolio and the latest service R&D programs for the SGT5-2000E gas turbine frame (formerly known as V94.2). These are particularly relevant to the needs of the African power market to optimize power output, efficiency and fuel flexibility. Measures to reduce overall maintenance effort and costs are also discussed.    

Presented at POWER-GEN Asia 2017

This paper shows the rise of cyber risk for industrial systems and presents how  plants can be protected and risks minimized within industrial automation. 

Presented at POWER-GEN Europe 2017

This paper will present Siemens solutions to actual customer situations for performance, profitability and risk management using monitoring, diagnostics and data analytics.

Presented at POWER-GEN Europe 2017

As steady state operation has become much less common for most operators, companies have to become more agile and lean in the way they operate, and pushing down fixed costs year after year has become a way of life.

This paper presents what can be done to make an energy company fit to compete in this very unforgiving climate, and to eliminate the issues that may lead to operational failure.

Presented at POWER-GEN Africa 2016

To increase the power availability of CCPPs after shutdowns of differing lengths, a number of improvements including variable gas turbine operating modes have been developed and tested, and are presented in this paper. It will be shown that it is possible to adjust startup capabilities of the CCPP fleet in service to changing market requirements.

Presented at POWER-GEN Europe 2017

Implementation of innovative design features and load-dependent air-pressure control enable SGen-2000P-series generators to achieve efficiency levels comparable to indirect hydrogen-cooled units while significantly improving flex power capability. This paper takes a closer look at the series’ design features and product benefits for new applications and retrofits.

Presented at POWER-GEN Asia 2017

This paper presents recent technology enhancements and ongoing development efforts to adapt the operational performance of fossil power plants to the demanding power generation market with very low leveled costs of electricity.

Presented at POWER-GEN Asia 2017

This paper describes the modules of the advanced maintenance for steam turbine valves, starting from the standard maintenance schedule, to the design and wear mechanism of the valve components, to the condition monitoring and risk assessment, to the influence on the inspection intervals and the overall availability of the steam turbine.

Presented at EPRI 2018

In this paper the successful implementation of GVPI to SVPI (Single Vacuum Pressure Impregnation) field rewinds on two gas turbine generators in parallel required after a forced outage of a 520 MW combined-cycle natural gas-fired power plant with delivery on time for the customer’s critical summer operating period is presented.  

Download technical paper

Presented at 9th International Gas Turbine Conference 2018

During the last years, Additive Manufacturing (AM) has emerged the industry and is considered as a game-changer. This technology enables OEMs to manufacture and repair gas turbine components faster and at the same time with enhanced functionality and performance. Currently Siemens is using this technology for prototyping, manufacturing, repair of gas turbine components, and spare part manufacturing. Industrialization of the AM technology and current accumulated field experience of AM manufactured components will be discussed in this paper.  

Presented at Plant Simulation Worldwide User Conference Germany 2017

The technical paper available for download explains the new setup of the burner manufacturing at the Siemens gas turbine plant Berlin (Germany) and gives background information, such as simulation data, for example, to further improve the burner manufacturing process. 

Presented at Global Power and Propulsion Forum 2017

Metal-based additive manufacturing (AM) technologies such as selective laser melting (SLM) have seen successful applications in the gas turbine industry over the past years. Siemens large gas turbine applications are used to demonstrate the development and industrialization of the design for Additive Manufacturing (DFAM).