TIA Portal Modules | from V13
050 Advanced Programming
The learning/training documents on TIA Portal have a modular structure and cover the following topics:
• Hardware Configuration
• Example Processes
• Basics of PLC Programming
• Visualization
• Advanced Programming
• Drives
They are designed for the SIMATIC controllers IOT2000EDU, S7-1500, S7-1200 and S7-300.
In this chapter, you will become acquainted with the use of software PID controllers for the SIMATIC S7-1500 with the TIA Portal programming tool. The module explains the call-up, connection, configuration and optimization of a PID controller for the SIMATIC S7-1500. It also shows the steps for calling the PID controller in the TIA Portal and integrating it into a user program.
In this chapter, you will become acquainted with the use of software PID controllers for the SIMATIC S7-1200 with the TIA Portal programming tool. The module explains the call-up, connection, configuration and optimization of a PID controller for the SIMATIC S7-1200. It also shows the steps for calling the PID controller in the TIA Portal and integrating it into a user program.