Save time and improve quality in plant design

With COMOS Isometrics and solutions for 3D integration
Errors in plant engineering can be costly – especially if they impact on assembly and commissioning. Making things harder is the fact that plant engineers have to work together across multiple locations in today’s age of globalization. COMOS Isometrics and our solutions for 3D integration guarantee optimum quality when implementing process data at the geometric level – regardless of location.
Combining isometry and 3D to create an efficient process
Isometry is more than just a means of communication between process engineers and pipeline engineers. It’s also the link between various disciplines and departments involved in the creation and, subsequently, the operation of a pipeline system. COMOS Isometrics and our solutions for 3D integration combine the individual plant design stages to create an efficient process.Generate interactive isometrics from construction to as-built status with COMOS Isometrics
COMOS Isometrics is an optimal and complete solution for interactive isometry creation and is based on the central database for COMOS. Consistent data, intelligent data transfer, and support for different isometry types substantially reduce the risk of error – whether it is for a planning project such as new plant planning, reconstruction engineering, inventories or inspections.