What buildings make possible
With around 90% of our lives spend indoors, it is crucial that we feel comfortable and safe in buildings. At the same time, buildings account for around 40% of all energy consumption globally – with our systems and products, we offer solutions to make your building a perfect place – without compromising in comfort or safety – but at the same time to making your building more efficient – in terms of energy and performance.
The requirements for buildings of the future are high. They should offer all the possible amenities, use energy as efficiently as possible and not harm the environment. They should be safe and protect their users from fire and other hazards. And most importantly: They should be flexible.
Come and visit our booth in Hall 10.2 during the ISH 2019 and experience live, how – with the right building automation products and systems – you can turn buildings into smart buildings.
Cloud operations
Multiple innovations in the field of cloud- and IoT will be shown at the ISH. For example the new Building Operator: The fully scalable software solution is a cloud application, which enables not only control and service of a fleet of sites remotely. More importantly, it lets service providers resolve issues before occupants are affected. The 24/7 monitoring of your buildings’ data will lead to a faster event response – and in the end a higher customer satisfaction. The new X300 Gateway ensures secure connection of the sites to the cloud, keeping data save & secure. Building Operator, as well as already well-known solutions like Synco IC and Climatix IC, are now powered by Mindsphere.
Intelligent Valve
At the fair the new Intelligent Valve range, our first self-optimizing, dynamic valves with cloud connection for heating groups and air handling units will be presented. The new range of valves controls the flow rate, measures temperature and output and adjusts the valve settings to the heat exchanger. The devices can be configured in the cloud and be put into operation quickly and error-free by connecting via an app and Wi-Fi. Another benefit is the possibility to mount them flexibly, aligned to the space available. The flow sensor, valve and controller box can be mounted separately. Thanks to the option of loading additional functions from the cloud at any time, the Intelligent Valve always remains up-to-date.
Building management for small and mid-size buildings
Desigo CC Compact, which was launched in the fall of 2018, will make its trade fair debut. The compact version of Desigo CC includes all essential features in one software package and was specially developed to meet the functional requirements of small and mid-size buildings. Utilizing the modular Desigo CC platform, Desigo CC Compact is adaptable and can be expanded as needed. Read more here.

Cyber Security – a pillar of our digital world
Digital connectivity is making our lives easier and boosting business competitiveness. However, the risk of cyberattacks is increasing as well, causing governments and companies to join forces in defense.

Buildings and beyond
The business of firms in building automation, construction and real estate will experience substantial changes in the years to come. Digitization and artificial intelligence basically affect all industries to different degrees.