Cloud-based app for micro-breweries
Australian craft brewers are passionate about brewing, not operational technology. Still, there was a way for Siemens to win them over with MindSphere, the leading industrial IoT as a service solution and part of the Xcelerator portfolio.

Ready for Hannover Messe 2022
Visit us at Hannover Messe from May 30 to June 2, 2022, and experience firsthand our motto for the trade fair: “Let’s combine real and digital worlds for a sustainable tomorrow.”
Register today for your free ticket and to take advantage of other great event offers.
We’re ready to see you once again and for inspiring conversations!
When the yeast consumes the sugar to produce alcohol: That’s when the flavour is developed. It’s when beer becomes beer. Australian craft brewers are passionate about brewing, not industrial operational technology, yet Leonie Wong and Rex Chen from the MindSphere team still managed to make the data work for them; they want to always land the perfect brew and waste not a single drop.
In this market, Deacam, an Australian original equipment manufacturer (OEM), which provides automated brewing equipment and solutions to microbreweries, was looking to differentiate itself. Leonie Wong, responsible for Vertical Sales for Food & Beverage for Siemens Australia, and Solution Architect Rex Chen met with Deacam and their customers, the microbreweries themselves.
Brewing beer with consistent flavor
“The beer must go through a temperature behavior over several weeks. For a brewery, it is critical to ensure that they can replicate that temperature behavior time and time again, because that is what creates a consistent flavor,” explains Leonie Wong. Variations could lead to an entire brew of several thousand liters to go to waste. “To craft beer brewers, that would be a crime!” Leonie Wong says.
Once it was understood that data around fermentation is a priority, MindSphere was the perfect fit to start creating a solution tailored to the requirements and budged of craft brewers.
Capturing the perfect brewing temperature
In the previous systems of temperature capture that the brewers were using, the drift in the temperature range was too large. With MindSphere, the temperature data is digitized at the point of capture and added to application. What the team found was that this allows the brewers to more precisely track and control the fermentation vessel temperature.
The solution also provides historical data, so brewers can identify a temperature profile across historical batches, allowing them to locate and replicate their perfect batch in the future. The application contextualizes the data, to allow brewers to know exactly what is going on and make better decisions. This also means that when new equipment and tanks are added, it is pretty much a plug-and-play process, making it easier to expand operations.
“Deacam placed a lot of trust in us, giving us open access to their customers, KAIJU! Beer and others,” says Leonie Wong. “To have that triangular conversation – with Siemens, the OEM, as well as the end-user, the brewery itself – that is a valuable thing.”
Complete MindSphere app for the fermentation
With the feedback Deacam received from their customers the team was able to make a complete MindSphere application for the fermentation process called Fermecraft. Deacam now standardized their full control cabinet design using Siemens. Meanwhile, the application is still evolving and expanding to include features beyond fermentation.
“Over the last nine or ten years, we have seen the Australian craft brewing sector grow from about 12 breweries to approximately 600, and there are a number of OEMs that supply this market,” says Leonie Wong. “We are seeing this kind of tailor-made approach to new business and innovation as a new opportunity.”
For Leonie Wong, asking the right questions is what made the project successful. At times, both Deacam as well as the breweries themselves were not sure what they wanted and trying to define an accurate user requirement specification came down to the team’s ability to just sit down face-to-face with all the stakeholders and ask good quality questions.
Agile project to be quick, affordable, and painless
“We are moving towards an agile based project execution, where the idea is really about trying something quickly, something that is affordable and painless, to make sure that there is value and the customer is getting what they want, and then scaling from there,” adds Rex Chen. “Even for larger customers, we need to think in a way that is nimble.”
Deacam are specialists in modern electrical engineering. The company’s expertise has become the launching ground for automated operations of distilleries, breweries and wineries in the Yarra Valley, Victoria, Australia. The unique design concepts are now being used throughout Australia and even overseas.
Brothers Nat and Callum Reeves established themselves as the original hopmasters in 2013 in Melbourne, Australia. Since their first beer (Aftermath Double IPA) single handedly caused a statewide shortage of Simcoe hops, their hop-driven styles and unique branding have seen them grow the brewery and stay 100% family owned.
Kaiju means “strange creature” in Japanese. The tribe of kaijus of the brewery include the Diatamatic Hopzilla, Cthulhu, Behemoth, Betelgeuse and Hopped Out Red.
Fermecraft – using the latest Siemens technology, including MindSphere – digitalizes temperature data and captures it in our cloud-based platform. At KAIJU! Beer, the Siemens operator interface, programmable logic controller and MindSphere are working together successfully to control the fermentation vessel temperature by implementing chiller control. This makes production improvements faster and decision making easier – ultimately leading to improved and consistent quality. Through this new solution, microbreweries can now correctly capture variables, establish scalable technology, collect and analyze data efficiently and ensure ongoing improvement of processes and automation.
May 2020
Subscribe to our Newsletter
Stay up to date at all times: everything you need to know about electrification, automation, and digitalization.