Twin brothers create digital twins
Before an airplane takes off, you want to know for sure that it’s going to do fine, even in the harsh environments up in the air. At RadioBro Corporation, the Becnel brothers – twins themselves – develop aircraft electronics for their customers to provide that assurance.
“I wrote in my third grade journal that I wanted to be an aerospace engineer,” says Eric Becnel, Vice President and Chief Engineer of RadioBro Corporation. In his childhood all signs pointed up into the sky. “Our parents are both computer science majors and met at university, our father is a private pilot, and we all used to go to air shows.” With his twin brother Mark at his side, Eric’s wish came true. When they graduated, the two Masters of Science in Aerospace Engineering founded RadioBro Corporation.
The place to be for aeronautics-lovers
The brothers’ company is based in Huntsville, Alabama, a development hub for NASA, an engineering mecca in the U.S. and the place to be to develop ideas, design, and manufacture aerospace systems. It’s a very challenging market because our customers are very aware of the state of the art, as Mark Becnel knows. The President of RadioBro affirms that, “They’re extremely passionate about telling you what they want and what they don’t like.” RadioBro designs and produces aviation, orbital and industrial electronics systems, focusing on plug and play data acquisition technology.
Up in the air and in other harsh environments, that’s where the electronics systems from RadioBro are proving their USPs best. “We offer kitted solutions that collect data, connect machines, and distribute the data,” Eric says. “The devices take measurements, store them, and display them on a website in real-time. Temperature, pressure, stresses: These are just three examples of the measurements taken by our instruments. And these data can verify the engineering of anything.”
Under the name “Cyclone,” RadioBro brings the Internet of Things (IoT) into the expensive aircraft test market, the two owners explain, typical test preparation can take up to two months, but with Cyclone, testing has been reduced from months to weeks, resulting in faster time-to-market and significantly reducing testing costs for their customers.
Measurements in the air and on earth
While Cyclone for aerospace applications operates at up to 23,000 feet in altitude (so far), Cyclone for industrial applications works just as reliably on ground level. Here the system also might measure pressure, vibration, and temperature on a machine or on an assembly line in manufacturing. “This is important for companies that want to upgrade their equipment to the IoT, which allows an operator to monitor all of the equipment’s parameters and its performance,” Eric says.
These industrial customers once only received updates based on a manual inspection. “Now with the easy to install Cyclone, the measurements are automated, and they are able to receive the data immediately.” If something goes wrong, operators onsite and remotely will find out much sooner than in the past.
Familiar with the twin concept
Being twins themselves, it might not be a coincidence that digital twins play a crucial role in the Becnel’s business. “The fact we have access to and are familiar with the CAD system Solid Edge was key in our original business plan,” Mark recalls. “This was a key enabling factor from day one.”
Measurements in the air and on earth
While Cyclone for aerospace applications operates at up to 23,000 feet in altitude (so far), Cyclone for industrial applications works just as reliably on ground level. Here the system also might measure pressure, vibration, and temperature on a machine or on an assembly line in manufacturing. “This is important for companies that want to upgrade their equipment to the IoT, which allows an operator to monitor all of the equipment’s parameters and its performance,” Eric says.
These industrial customers once only received updates based on a manual inspection. “Now with the easy to install Cyclone, the measurements are automated, and they are able to receive the data immediately.” If something goes wrong, operators onsite and remotely will find out much sooner than in the past.
CAD with three major benefits
Using Solid Edge software has many advantages for RadioBro. “It is affordable and flexible, the intuitive user experience reduces the training time and enables the use of more powerful features, and the powerful features allow for rapid design-for-production used in supplier management,” Mark summarizes.
Cost of ownership
“Every small business has to be risk averse in order to change the way business is done,” Mark claims. “A monthly subscription to a reasonably priced software helps. Even small companies like startups can afford software with the little bit of money they have. And they don’t have to put themselves at risk,” he adds.
“The licenses for Solid Edge were much more affordable than any of Siemens’ competitors,” Mark says. “Siemens also guarantees that we can migrate our files, and access more advanced versions of the software through subscription licensing as needed without having to make a capital investment.”
Design for Production
The engineers develop all of their products using Solid Edge. The software comes in very handy: For example, if a supplier asks for a different tooling requirement, the change can be digitally modelled, interferences evaluated, and assembly simulations executed. The 3D models are very useful on our scale of tiny and highly integrated devices.
However, most of RadioBro’s suppliers and customers work with 2D drawings. “We can update the 2D drawings in less than 30 minutes,” Mark says. “And we can push all the updated drawings to our supply chain and get the project on its way. Firms like ours would usually work with a red-line modification, and the next time we’d do a major modification we’d update the drawings.” Now RadioBro can do it right away, in real time.
Whether it’s needed for integration with an aircraft or production of component in a factory, the actual time needed to install the RadioBro solution is critical, because the equipment must be switched off during installation. The advanced tool that RadioBro uses now saves the customers and suppliers time and money. “We learned this lesson on our first-generation product development and deployment,” Eric says. “
After developing and selling the second-generation Cyclone system, RadioBro now spends far less time at their customers’ sites, and the product works much better in operation, and remains much longer in the field. “Today, our customers’ experience is much more streamlined and easy,” Eric says.
More to come with new functionalities
Mark and Eric wouldn’t be ambitious aerospace engineers if they didn’t have high expectations of the tools they work with. “We always want to see continuous improvement – that keeps us competitive and increases our opportunities,” Mark says with tongue in cheek. “A big thing for us is getting the customer’s approval. This process has also become digitized. We are just starting to use the new built-in data management. This is going to help us a lot, because it means that no one would have to leave the software as soon as the customer gives us their approval.”
The integration of Mentor Graphics into Solid Edge is also eagerly awaited by both company owners. “One of our new requirements is thermal analysis, so we’re very excited to start using the new FloEFD tool with Solid Edge,” Eric says. Mentor Graphics will also be used for integrated circuit design, because the engineers are constantly working with multiple circuit cards. “The ability to work in an integrated environment will help us work more efficiently and help us decrease our time-to-market even further,” Eric says.
Solid Edge for Startups
RadioBro participates in the Solid Edge for Startups program that provides Early-stage startups with free use of Solid Edge Premium software for a whole year. The companies also have access to Solid Edge training resources and guidance from an online community of product experts. If RadioBro’s revenue is strong enough after this year is over, they can easily maintain their software and scale it to their needs with a monthly subscription.
Solid Edge ST10 is already on RadioBro’s horizon. “It is changing the way products are designed entirely, and is making our quality system more efficient,” Mark says. “In my opinion, it’s still a too well-kept secret, if you consider the capability of it.” We’ll see if the new generative design tool meets – or even exceeds – the twins’ expectations.
Startups have to get products and services to market as quickly as possible. CAD software is key to achieving this goal. Siemens launched the Solid Edge for Startups program, which is open to early-stage startups in business for less than three years.
Applicants can use Solid Edge Premium for a whole year and get one licence for each engineer. The startups have access to Solid Edge training resources and guidance from a community of product experts.
Solid Edge for startups is currently rolled out in 33 countries, after having had their initial launch in the U.S. and Germany.
RadioBro is a design and manufacturing company that provides miniature electronics systems for aerospace and industrial customers. The team leverages technology and product design techniques from the nano and pico class of small spacecraft along with space-grade testing. And thanks to the stringent quality system required for aviation production, RadioBro supports the most challenging engineering tasks.
March 2018
Photos: Mike Mercier, UAH, Mark Becnel
Subscribe to our Newsletter
Stay up to date at all times: everything you need to know about electrification, automation, and digitalization.