TIA Portal Modules | from V13
060 Drives
The learning/training documents on TIA Portal have a modular structure and cover the following topics:
• Hardware Configuration
• Example Processes
• Basics of PLC Programming
• Visualization
• Advanced Programming
• Drives
They are designed for the SIMATIC controllers IOT2000EDU, S7-1500, S7-1200 and S7-300.
In this chapter you learn how a frequency converter SINAMICS G120 with the Control Unit CU250S-2 PN Vector and together with a CPU1516F-3 PN/DP on PROFINET is put into operation. The module explains the basic commissioning of the frequency converter SINAMICS G120 with the SINAMICS Startdrive software in the TIA Portal. Subsequently we show step-by-step how the frequency converter SINAMICS G120 can be controlled and monitored from the program of the CPU1516F-3 PN/DP.
In this chapter, you will learn how a SINAMICS S210 PN frequency converter can be commissioned with a SIMATIC S7 controller – based on the example of a CPU1516F-3 PN/DP with PROFINET IRT (Isochronous Real Time). The module explains the commissioning of the SERVO drive system S210 PN with the SINAMICS Startdrive software in the TIA Portal. Subsequently, we show step-by-step how the servomotor from the program of the CPU1516F-3 PN/DP can be controlled and monitored via technology objects.