TIA Portal Modules | from V13
020 Example Processes with SIMIT Models
The learning/training documents on TIA Portal have a modular structure and cover the following topics:
• Hardware Configuration
• Example Processes
• Basics of PLC Programming
• Visualization
• Advanced Programming
• Drives
They are designed for the SIMATIC controllers IOT2000EDU, S7-1500, S7-1200 and S7-300.
The following pages will show how a coupling with a SIMATIC S7-1500 program can be set up in PLCSIM Advanced via TCP/IP in the SIMIT process simulation software. The order in which the existing SIMIT projects with this coupling variant can be started together with a TIA Portal project for simulation will also be described.
The following pages will show how a coupling with SIMATIC S7-PLCSIM Advanced via OPC UA can be set up in the SIMIT process simulation software. The order in which existing SIMIT projects with this coupling variant can be started together with a TIA Portal project for simulation of a program solution will also be described.
The following pages will show how a coupling with a SIMATIC S7-1500 via OPC UA can be set up in the SIMIT process simulation software. The order in which existing SIMIT projects with this coupling variant can be started together with a TIA Portal project for simulation of a program solution will also be described.