A natural choice

Success in challenging markets – with Siemens LNG solutions. The entire LNG value chain places high demands on safety and efficiency, and requires highly reliable technologies that make both operators and investors happy.
Energy World Corporation

Siemens LNG solutions: the power of efficiency

Based in Hong Kong, integrated energy company Energy World Corporation (EWC) is looking for solutions that unlock efficiency potentials in their primary gas, LNG and power operations.

Less is more: LNG solutions made to measure

For EWC’s planned Sengkang LNG operation in Indonesia, there was no standard equipment available. So the company designed a modular system that allows smaller LNG plants to be developed far more economically. At the core of the concept: a Siemens all-electric LNG solution, comprising compressors with electric drive systems for four 0.5 MTPA liquefaction trains, that significantly increases cost effectiveness in construction, operation and maintenance.

When all the calculations were done, the actual efficiency of running the plant with Siemens LNG solutions was somewhere around the 46-50% as against something like 30% or 32% on some of the others.

Stewart Elliott, CEO Energy World Corporation, LTD.

OLT Offshore LNG Toscana

Siemens LNG solutions: safe and sound

Floating LNG storage and regasification terminals like the “FSRU Toscana” require sturdy rotating equipment and a reliable and efficient solution for boil-off gas compression.

Performance on the high seas: LNG solutions for offshore service

OLT Offshore LNG Toscana S.p.A. (OLT) is the company that developed, and now owns and manages, the floating regasification terminal “FSRU Toscana”. The mission of OLT is to provide LNG regasification service to support the Italian natural gas grid in times of peak demand. During the storing of cargo from visiting ships and the regasification process, a lot of boil-off gas is created. A Siemens LNG solution based on a boil-off compressor helps keep these transfers safe and allows the gas to be sent ashore instead of being vented or burned. The result: less environmental impact, increased efficiency and reliable gas supply for the Italian mainland.

The boil-off gas compressor is a core part of our terminal, making it possible to have an offshore terminal that performs as well as a traditional onshore terminal during the offloading operation.

Giovanni Giorgi, Operation & Maintenance Manager “FSRU Toscana”

How is the LNG market evolving? Michael Stoppard has answers.

Read interview

Solution

Engineering ingenuity for liquefied natural gas

With a broad range of technologies, including electrification, compression and process automation, Siemens ensures efficient, reliable and safe LNG plant operation. As an option, fully packaged functional modules help to meet space and weight requirements for offshore service and support project economics in challenging onshore construction environments.
Portfolio overview

Safety, efficiency and reliability along the entire LNG value chain

Reliable Siemens technologies are a natural choice for LNG plant investors and operators. Learn more about our comprehensive portfolio.