Deburrer tool
Professional tool for daily use - self-made
The workpiece
Solid and practical: The robust hand deburrer is a professional tool for daily use during manufacturing. It uses commercially available blades and its shaft has a screwable compartment for spare blades or alternative blade types.
The hand deburrer consists of three turned parts which can be manufactured without any additional fixtures. The head part and the knurled screw at the back are made of brass, the handle is made of steel. Purchased parts are the deburring blades and a grub screw.
The tool data and NC programs (ShopTurn work plans) required for production are listed below.
Note
The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.