Modular ballpoint pen with engraving
Material mix of aluminum, brass and/or plastic, two lengths
The workpiece
This modular ballpoint pen fits well in the hand and can be manufactured in a material mix of aluminum, brass and/or plastic, in two lengths for different hand sizes, and with a personal engraving. The ballpoint pen was developed by the BBS-Burgdorf Vocational Schools in Burgdorf, Germany. It is custom made and awarded on special occasions.
The ballpoint pen, crafted from six individually turned parts, is a pleasure to use.
All information required for the reproduction, tool data, drawings and ShopTurn machining plan are summarized in the following sections.
Note
The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.