Simulation and virtual commissioning with TIA Portal

Reduce time and risk in machine building and plant engineering and lay the foundation for new business models
Faults are inevitable during the development of a machine or plant. However, they can cause high costs and enormous effort when they are only detected during real commissioning. Integration in a line or plant involves risks as well. A solution is simulation with TIA Portal. Based on the digital twin of a new machine or line you’re able to parallelize engineering, test functions and detect faults earlier, simulate the interplay of the machine in a line, and optimize operation while its running. Also, additional services can be offered based on the digital twin of the machine, which can also be used for marketing, i.e. at fairs or in a virtual showroom.

#PackTalks Vol. 4 - Simulate & understand complex relationships in packaging machines
Practical introduction - multiphysics simulation with Simcenter Amesim
In our webinar we talk about a tool from our digitization portfolio with which you can model, simulate and optimize multiphysics.
The target group for the webinar are electrical and mechanical construction as well as automation technology.
Save time and money with virtual commissioning
You can play it safe right from the start by using the digital twin of a machine or line: from the concept phase to development to commissioning and optimization during operation. Thanks to simulations and virtual commissioning you’re able to reduce the time to market of new machines and lines, reduce error costs, increase quality, and reduce risks during real commissioning.Test engineering and simulation software for free
Continuing to work on machines and promote development despite being in the home office? This is possible with engineering and simulation software in the cloud.
Test our cloud-based development environment and discover the benefits for building new machines or production lines that our simulation know-how has to offer.
Get your free trial version now!
The virtual machine
In order to fully digitalize a machine, it’s necessary to virtualize its three essential elements: automation, electrics, and mechanics. SIMATIC S7-PLCSIM Advanced represents the virtual controller based on the SIMATIC S7-1500 and is required for simulation of the controller software. An open interface lets you connect the virtual SIMATIC controller to a variety of other simulation tools. An example is SIMIT, which represents the electrical behavior. In order to complete the digital twin of machine it’s necessary to include and simulate mechanics and kinematics. This is a task for NX Mechatronics Concept Designer.
The virtual production cell
Before integrating a machine into a production line, it’s possible to validate the interplay of a superimposed controller with robots and the creation of complete robot programs. This facilitates the design of cells and the validation of workflows in complex manufacturing lines with many interacting robots.
The virtual line
The virtual line comprises several simulation models: a discrete event-oriented simulation model that simulates material flow. A communication model that comprises interfaces to automation and third-party tools. And an automation model that enables to simulate a controller.
For machines with SIMATIC S7-1500
Simulations are also useful to optimize machines during operation. This way you can realistically verify and validate the automation in complex mechatronic systems and processes, even if the hardware configuration isn’t finished yet. Fast simulation cycles and synchronization also enable optimizing the control strategy including closed-loop applications like PID controllers.
Request the whitepaper here
Shorter time-to-market, cost reduction, better quality, and increased flexibility to adapt to market changes – most industrial companies must face big challenges, and digitization seems to be the answer. However, the variety of topics makes it difficult for companies to find the right way: The digital twin is one of them and can already exert big impact now, and over the entire life cycle! So read how you also can place the digital twin at the beginning of the digital transformation of your automation processes and see how AFRY's engineering services and Siemens' Digital Enterprise Portfolio offer an easy start with fastest return on investment.Learn more
Simulation in a virtual environment yields real-world benefits
The virtual commissioning of controllers, HMIs, machines, and production lines decreases time and costs, reduces the risk of errors and defects, and achieves the desired results more quickly. With TIA and the TIA Portal as the engineering framework, you have access to all the relevant data on your hardware and the software tools that will enable you to develop, simulate, and optimize in a completely virtual environment.