Insys

Smoke detector automatically produced with SIMATIC HMI

Insys Industriesysteme AG in Muensingen, Bern, uses SIMATIC HMI Mobile Panels in an innovative, fully automatic assembly system for smoke detectors.
Yes I want to know more about SIMATIC HMI - Efficient to a new level

Contact us!

Challenge

Modular solution for complex processes with high precision

Every 4.8 seconds, the system produces a smoke detector in its final configuration: The new modular production process is a real challenge for automation. The sensitive electronic board must be broken out of a carrier and mounted. The handling of the LEDs is just as demanding.

Modular system concept to combine precision and expandability

At the various stations of the new assembly system, it is possible to observe how smoke detectors are created. The base carrier is manually fed into the system - after which the automatic system takes over. The electronic board is used at the beginning of the assembly system.

The carrier is turned over and placed on the rotary table, where eight stations assemble the other components: 1-2 light-emitting diodes, a photodiode, the shield plate and the lens.

Speed and reliability are central to the manufacture of the smoke detectors: in order to make the system faster, more flexible and cheaper, only electric axes were used, and pneumatic components were dispensed. This also reduces energy consumption. The automation stations for lid assembly and packaging are added later.

Thanks to the modular design of the system, the manual feeding of the base carrier can also be automated. The requirements for the operating solution for the system were correspondingly high: The HMI should optimally support the personnel in the control, optimization and maintenance of the system and at the same time be flexibly adaptable to new tasks.

Insys Industriesysteme AG

Smart solutions for complex and cross-linked automation

Insys Industriesysteme AG (member of Smart Automation Group) realizes special machines for medical and electrical engineering, the luxury industry and the automotive sector. The 70 employees in the Bernese town of Muensingen develop grinding, polishing and testing systems and in particular complex assembly systems - such as the new system for the production of smoke detectors.
We have implemented a more extensive system, which can be further expanded modularly.
Marc Luginbühl, CSO, Insys Industriesysteme AG
Solution

Flexible and integrated

For the automation of the plant, Insys used Siemens components consistently: From the HMI operating device and a software controller on a SIMATIC industrial PC to safety circuits and SIMATIC ET 200SP peripheral modules.

Complete automation solution from the same source

The Teamcenter Lifecycle Management (PLM) platform is used for optimal data management. The powerful Scalance Ethernet Switches enable a quick and easy setup of networks. The high-end motion control system SIMOTION convinces through its performance and enables a high flexibility of the assembly system, and SITOP components ensure a reliable power supply of the system. The system is operated via a 4-inch mobile panel from Siemens. The SIMATIC HMI mobile panels communicate via Profinet and are fully IP65 protected. Safety Integrated guarantees the safety of the system and employees. Together with the connection box, it forms a space- and cost-saving solution for tasks with safety-relevant operating functions that do not require complex graphical representation. 4 function keys support touch functionality for combined touch and key operation.

Benefits

The mobile panel from SIMATIC HMI impresses with its high functionality, compactness and flexibility. Marc Luginbuehl is enthusiastic: "The handy panel has all the necessary functions, is attractive, compact and easy to operate".

Regarding the engineering, Insys benefited in particular from the seamless integration of all automation components in a common framework: The TIA Portal provides corresponding software modules that greatly simplify programming. Using the Teamcenter Product Lifecycle Management (PLM) platform, design data can be optimally managed. An efficient development across company boundaries becomes possible. Of course, the project data from the TIA portal can also be integrated into Teamcenter. In the future, the system will be connected to the IT system from Siemens Building Technologies. The continuously exchanged data can be used for quality assurance or order planning. As a result, Marc Luginbuehl draws a positive conclusion from his experience with the integrated solution from Siemens: "It is quite possible that we will be using the panel and other Siemens components more frequently in the future".

Portfolio

Complete solution for innovative assembly system

For the new smoke alarm assembly system at Siemens Building Technologies, Insys used various components from industrial automation and production IT. The seamless integration of the different systems simplifies the engineering, operation and maintenance of the system.
Further references

SIMATIC HMI – Used everywhere

Contact

What does your mobile solution look like?

Do you want a HMI Mobile Panel or Tablet PC to be optimally prepared for everyday industrial use, whether in production or at your desk? Our experts will be happy to help you!

We are looking forward to advise you on your individual mobile solution.

Contact us!