SINUMERIK ONE – the No. 1 for machine tool users

SINUMERIK ONE convinces through the advantages that the digital twin brings to machine manufacturers and users. The virtual image becomes the reference variable for real action. Quality and speed in the production of the workpiece also count. Read here which benefits SINUMERIK ONE offers to machine users.

All information about SINUMERIK ONE at first hand!

Stay up to date

Logos Media Center

All SINUMERIK ONE references at a glance

Find out more about the experience of numerous machine tool manufacturers with SINUMERIK ONE.

Benefits of the digital twin

Digital First with SINUMERIK ONE

SINUMERIK ONE enables a consistent “digital first” strategy. This means that key manufacturing processes (e.g. programming, job preparation or process optimization) are always simulated first using digital twins, in other words, on detailed virtual images of the controls and machining. The result is faster communication with customers about prices and deadlines, more accurate planning and job preparation, and increased productivity, even with falling batch sizes and an increasing range of variants.
The benefits of the CNC control

Improved performance on the shop floor

SINUMERIK ONE is optimized for performance. An innovative system architecture means the system will impress with its excellent productivity. In the highly demanding area of mold making, in particular, double-digit productivity gains are a real possibility, depending on the machine. Innovative software functions leverage the potential of the latest processor technologies, so very different processing functions can be run in parallel without performance losses.

Ideal for modular and also for compact machines

SINUMERIK ONE is available in several control cabinet-based NCU variants as well as in a compact panel-based PPU (Panel Processing Unit) variant. The PPU version combines the CNC control and a 15'' or 19'' HMI panel in one component. This makes SINUMERIK ONE suitable for both modular and compact machines.

Technology packages

SINUMERIK ONE Dynamics – powerful new technology packages

Options for efficient CNC programming on the shopfloor and execution of CAM-generated CNC programs

SINUMERIK ONE Dynamics offers a series of options for your machine tool with three complementary technology packages:

  • SINUMERIK ONE Dynamics Operate
  • SINUMERIK ONE Dynamics 3-axis milling
  • SINUMERIK ONE Dynamics 5-axis milling

Jobshop

Tool and mold making

Plant managers

SINUMERIK ONE for machine tool builders

Discover a new way of thinking

Find out more about the benefits of SINUMERIK ONE in engineering and commissioning and how the CNC increases the performance of modern machine tools.
Information

SINUMERIK ONE and more

Learn more about the many benefits that SINUMERIK ONE has to offer. Get continuous updates on the latest news and first reports on SINUMERIK ONE.