Do it right: Dynamic hydronic balancing

Dynamic hydronic balancing

We have a responsibility to create buildings that are better for people and that are sustainable for the environment – and that means transforming buildings into environments that care.

Buildings consume about 40 percent of all energy worldwide, and HVAC systems account for more than 40 percent of buildings’ energy usage. That’s why optimizing HVAC systems is essential for the future. But people don’t want to compromise on comfort – so we need to build energy-efficient HVAC systems that adapt to peoples’ needs and keep comfort at the highest level. Hydronic flow optimization is a prime way to reduce HVAC energy consumption while also increasing overall building efficiency and operational performance.

Learn how to create energy-efficient HVAC systems with optimized hydronic flow that deliver the highest level of comfort: dynamically balanced hydronic systems

Why balance a hydronic system?

Water always flows through the path of least resistance.

However, the HVAC system’s pipe network in buildings is highly branched and contains pipes of different diameters. This means that the water and therefore the heat are distributed unevenly, and some consumers get more heat than others. The consumers farthest from the pump are supplied with too little heat, and those nearest the pump get too much. As soon as one room occupant turns on the heat, another area of the building will inevitably get less heat. This leads to unstable room temperatures, and the comfort of the occupants is impaired. Energy is wasted and unnecessary costs are triggered by excessive and unnecessary heating/cooling.

 

Hydronic balancing can prevent this situation from occurring. The simplest definition of hydronic balancing is:

The right amount of water at the right time in the right place

Sounds easy! But is it?

It means that the water is distributed in the optimal way. With hydronic balancing, all components in the hydronic system are matched and balanced, ensuring that energy is distributed evenly throughout the system. There are several ways to create a balanced hydronic system. Watch the following two videos to explore the most important differences or read the explanation below:

Summary flyer

Download the summary of the comparison of standard control valves and dynamic valves

In other words: Dynamic balancing is the right way to do hydronic balancing

Have a look at the following video and learn how digitalization expands the context of dynamic hydronic balancing.

Dynamic hydronic balancing applications

Have a look at the video below regarding the overall main applications offered by dynamic hydronic balancing and scroll the slider to watch detailed episodes for each application.

Additional functionalities

Valve and pump interactions

Explore the interactions between valve and pump by clicking on the video below. Scroll the slider to watch what needs to be done during the commissioning phase.

How to select a valve?

Click on the link below and find several examples for valve selection with PICVs and with standard control valves.

ff

More hydronics knowledge

Tune in and listen to the podcast about hydronics in our Buildings of Tomorrow series. Get your weekly insights on industry trends and innovations which make the buildings safer, sustainable, and deliver more productive and healthier environments.

Contact

How can we help you?

If you have questions, comments or feedback, please feel free to contact us. We're ready to help!