Where can I find a subsidy for my battery? An overview.

May 2019

Where can I find a subsidy for my battery? An overview.

State subsidies reduce investment costs for energy storage and increase their cost-effectiveness. But what states and municipalities actually offer these subsidy programs? What are the requirements, and how high are the subsidies? We’ve put together an overview.

Varied subsidy landscape

The Germany-wide subsidy program “Renewable Energies – Storage” offered by the Kreditanstalt für Wiederaufbau (KfW) was discontinued on December 31, 2018. However, there are many new local subsidy programs to promote grid stabilization through the installation of distributed storage systems – so you can still benefit from a subsidy for your energy storage!

 

In particular, subsidy programs are currently (May 2019) being offered by Baden-Wuerttemberg, Bavaria, North Rhine-Westphalia, Saxony, and Thuringia. Subsidies in Brandenburg are limited in number, and the quota is currently filled. There are also numerous municipal programs. It’s a good idea to regularly check the subsidy database to find out about the latest developments.

Subsidy Database

In Baden-Wuerttemberg, the Ministry has earmarked €10 million to provide financial incentives for purchasing “grid-relevant battery storage” in conjunction with a photovoltaic (PV) system in order to reduce the load on distribution grids. The subsidy conditions were last updated on February 1, 2019.

"Grid-Relevant Battery Storage” subsidy program

More information

Since 2015, the Free State of Bavaria has been subsidizing investments in energy storage as part of its 10,000 Houses program for energy-efficient building refurbishment and construction. According to a current statement by the Ministry of Economic Affairs, an additional, separate storage subsidy program is also being planned.

"10,000 Houses” subsidy program

More information

North Rhine-Westphalia has been subsidizing investments in energy storage in conjunction with a newly installed PV system since October 2018, as part of its “progres.nrw Market Launch” subsidy program.

“progres.nrw Market Launch” subsidy program

More information

The state of Saxony subsidizes private energy storage and its connection to charging infrastructures for electric vehicles for the purpose of increasing the consumption of self-generated solar electricity. Both new installations and retrofits for additional storage capacity are subsidized.

“Energy storage with/without Charging Station” subsidy program

More information

The state subsidizes PV systems and batteries for personal consumption of self-generated electricity through its Thüringer Aufbaubank. PV systems are subsidized only if 100 percent of the electricity produced is “self-consumed” and none is fed into the public grid. This is an excellent reason to purchase a large battery.

“Solarinvest – Subsidy for Consumption of Own Self-Generated Electricity” subsidy program

More information

Released by Pawel Nicinski