Fault reporting – fast, flexible, and direct

Fault localization in the cloud – the cloud-based service for fault detection by Siemens

The basis for fast and efficient fault management was previously bound to the control room. Fault localization in the cloud is a new, cloud-based service, which makes it possible to send fault information – including the fault location – directly to the maintenance crews, without the need for a grid control center.   The result is that fault messages are enabled even without a control room or complex IT hardware – making it a mobile and surprisingly cost-effective alternative. Discover the advantages of this solution now!

Modern city

European Utility Week 2019

Visit us from November 12-14, 2019 in Paris and find out how we are powering energy-intelligent societies.

Fault localization in detail

There’s no way around efficient fault management

Fault localization in the cloud is the latest service from Siemens for efficient, simple, and cost-effective fault localization. It can be implemented without an investment-intensive IT/OT infrastructure on the part of the network operator.

The safe and reliable supply of power for both industrial and private customers is now more in demand than ever before. Existing medium-voltage networks, however, have historically been very limited in the extent to which they pursue automation and intelligent methods. The result is unnecessarily high maintenance efforts, especially for grid distribution operators, and makes the essential interference management more difficult.

In case of a short circuit or ground fault, the power supply must be restored as quickly as possible. If an overhead line is damaged, fault localization is usually very complex. Maintenance teams must check the so-called fault passage indicators (FPI) along overhead lines, or route the individual substations sequentially in order to locate and correct the fault. Fault reporting systems significantly reduce the time needed for this process but are dependent on a control room.

Traditional fault management

In the event of a fault, a fault indication in the control room signals the response of the circuit breaker or disconnector in the affected line section. In doing so, it allows the staff in the control room to send a maintenance team directly to the identified fault location quickly and eliminate a complex, on-site search. 

For some time now, fault indicators were able to be equipped with a modem or a mobile radio gateway at the factory, then used for fault reporting. But to date, their signals were not able to be collected and evaluated without a control room.

Fault localization in the cloud – simply clever

The Siemens cloud takes on the role of the control room in the event of a fault localization in the cloud. All faults are automatically reported there, quickly evaluated, and transmitted to the maintenance personnel’s mobile devices, complete with accurate position data. Your advantage: Even without a dedicated control room, you have a sophisticated, efficient fault management that can be set up quickly and easily.

Available from anywhere and easy to use

The ability to perform fault localization in the cloud leads to comprehensive grid monitoring capabilities, all in a user-friendly Web browser-based plug-and-play solution, which is available on mobile devices at all times.

Operation is simple: Fault indicators are automatically logged in the cloud during installation by a QR code scan and the GPS coordinate. Then, the cloud signals the faults, displays the relevant fault indicators on a geographic map, and sends fault information messages directly to the mobile technicians’ mobile handsets. In this way, grid distribution operators can significantly reduce the time and effort required for fault localization without investing in the construction and maintenance of a complex IT/OT infrastructure.

Quick implementation

A set for fault localization in the cloud contains a pre-parameterized communication gateway and three pre-configured FPIs. The user simply logs in from the workplace in the cloud and stores the mobile phone numbers of his employees. No further installation work or additional mobile communications contracts are required. The fault indicators are automatically detected. With the help of the SIM card, they register themselves independently in the cloud and only have to be installed in the field on the respective lines and masts and registered in a few working steps.

This is how you profit from Siemens’ innovative offer

Modern technology used to your advantage – this is fault localization in the cloud. This allows you to quickly and easily optimize your fault management without having to invest in expensive technology.

Want to learn more about the benefits of fault localization in the cloud?

Download iPDF

Contact

Still have questions?

Contact us to find out how fault localization in the cloud can help your organization achieve optimal fault management.