Self Optimizing Grid

An innovative and smart solution

The power distribution grid is facing a unique set of challenges that are increasing pressure on an already struggling and ageing infrastructure. Distributed power generation, changing political frameworks, fluctuating peak times, and an increase in the number of consumers – or ‘prosumers’ – producing energy, are key contributors to a worrying trend that is likely to escalate in the future. As a measure to counteract this trend, Siemens has developed the Self Optimizing Grid; an innovative and smart solution that combines automation and decentralized applications to monitor and remotely control the grid.

Modern city

European Utility Week 2019

Visit us from November 12-14, 2019 in Paris and find out how we are powering energy-intelligent societies.

Levels of automation in distribution grids

Application of highest relevance

The self-optimizing solutions use grid automation to enhance reliability and availability of the power distribution system, which increases the efficiency of grid management and operation and improves the distribution system operator’s key performance indicators (KPIs).

Hierarchy of modern distribution grids

Distribution grids are made up of control centers, regional controllers, secondary substations and device groups and the actuation of each of these components depends on its hierarchical position in the grid. A modern distribution grid is divided into three levels: central, where control centers are located; semi-decentralized, where regional controllers are positioned; and decentralized, where secondary substations and device groups are found.

Application on different levels

The Self-Optimizing Grid is fundamentally a holistic solution that combines elements of each level of the distribution grid solution. Flexibility has been built into the solution at every level, which also allows for a modular approach that, through customization and adaption, efficiently meets individual needs. Self-Optimizing Grid solutions integrate the different levels of the grid and, depending on integration level, can be: centralized, semi-decentralized and/or decentralized. However; the more decentralized the solution, the lower the decision complexity and the faster the decision time.

In the specific case of a semi-decentralized architecture, the system robustness creates perfect balance with decision complexity, as network data flow is reduced. The system protects the control center from data overload scenarios by pre-processing data and taking decisions at regional control level, while only simple indications and pre-processed information is taken to higher levels in the system architecture. The system architecture also delivers extended cyber security through segmentation of access. This level of flexibility allows the application to be extended to different sections of the grid without being limited by the maximum capacity of the control center.

Self-Optimizing Grid relevant applications

Creating optimal performance

The self-optimized grid solution is comprised of the most relevant applications for semi-decentralized solutions. These applications accurately monitor the grid and remotely control stations to ensure high reliability of supply and improve system performance, using several intelligent functions.

Self-healing

The self-healing application reduces outage time through the early detection of fault location. The application’s algorithm identifies the location of the fault and isolates the damaged section; it then reconfigures the section by closing the normally open points of the grid to restore supply to consumers. Once the outage is cleared, the system re-establishes the network to its normal state.

Self-healing automation supports every type of standardized communication protocol and provides secure and reliable operation for these and essential primary equipment, such as circuit breakers, load breakers, disconnectors, reclosers and sectionalizers.

Self-Optimizing Grid process time is not reliant on the communication protocols and/or the calculation of the regional controller. It is largely dependent on the motorized mechanical switching time, which is performed in seconds, as opposed to manual switching which takes, on average, 120 minutes.    

Load Management

The objective of the Load Management application is to reduce the number of outages on the grid by automatically reconfiguring the feeder of a load to avoid overload on lines, transformers and switches.

  • Current overload triggers algorithm.
  • Automation system identifies normally open points.
  • Identifies overloaded section and connection to alternative sources.
  • System calculates potential additional load from alternative source.
  • Connects to source with largest spare capacity.

Automatic Source Transfer

The Automatic Source Transfer application automatically transfers critical loads to an alternate source in the event of a loss of voltage incident. Like Load Management, its main objective is to reduce the number and duration of outages on the grid.

  • Algorithm starts at under voltage detection of grid power source.
  • Automation system evaluates the segment connection to alternative source.
  • System connects to the source with largest spare capacity.
  • System disconnects last section in segment.
  • Connects with chosen alternate grid segment.

Overload Reduction

The primary function of Overload Reduction is to handle unmanageable loads on the grid. The application considers the load situation of the grid in a similar manner to Load Management application, but on the basis that load shifting to a different grid section or source is not possible.

Overload reduction is used to cut overloads on lines, transformers and switches and to reduce the unsupplied region to a minimum. It is used in radial grid structures where loads cannot be transferred, or in open ring structures where the interconnected ring is not able to take additional load. It successfully limits outage areas, depending on the possibilities of the operating scenario and the parameters of the objective function.

Area Voltage Control

The Wide-Area Voltage Application uses several intelligent secondary substations to monitor and regulate voltage level by measuring current and power flow to avoid voltage deviation of a minimum and maximum level. The algorithm creates a voltage level map by following the topology of the grid to establish the voltage value the algorithm must monitor, that is, the value required under normal conditions. Stabilization is performed by increasing or decreasing the step position (TAP) of the voltage regulator.

This application is used when load and generation are dispersed consistently in the distribution grid's primary transformer. It allows the line-voltage regulator and regulated distribution transformer to separate the grid into controllable areas, with minimal disruption to the rest of the grid. The aim of area voltage control is to reduce the cost of expansion of lines, and to support energy management for monitoring and planning purposes, while ensuring that compliance with standard IEC 50160.

Benefits

What can a semi-distributed solution offer?

Self-Optimizing Grid is an innovative and intelligent solution that allows customers to enhance their current infrastructure and optimize the grid, rather than investing in costly new assets.

It complies fully with International Standards, such as, IEC 61850, IEC 60870-5-104, or DNP 3 which govern digital communication for regional monitoring and control functions, and existing communication lines and protocols. Cyber Security is the highest priority for Siemens and is a primary focus across all operations; the solution is also in line with the Standard IEC-62443.

To ensure transparency across our solution, all applications are standardized and use the same remote monitoring and control devices of the distribution grid, and support all layouts of grid topology. Self-Optimizing Grid applications will effectively and equally support more rural networks that primarily operate with overhead lines, as well as urban networks that predominantly utilize cable infrastructure.  All applications operate successfully across medium voltage and low voltage grids alike.

The platform for the Self-Optimizing Grid application runs on proven substation automation equipment combined with intelligent field equipment.

References

Greater efficiency – thanks to perfectly tailored solutions

Download

Innovation and Automation

Sign up to receive more information on intelligent grid automation from a regional perspective with semi decentralized appliactions.

Contact

Your grid is our concern

Any questions about the challenges? Are you looking for products, solutions, or specialized knowledge? Let our grid experts help you to find the optimal solution for your specific requirements.

Individual consulting and customized solutions

Contact our grid specialists