Frequency and voltage support for dynamic grid stability

SVC PLUS (STATCOM) Frequency Stabilizer

As the infeed of power from renewable sources continues to replace conventional synchronous power generation, the grid frequency is becoming more sensitive due to the reduced amount of rotating machines. Now grid operators are faced with the challenge of providing sufficient system inertia in their synchronous generators with high rotating masses to stabilize the grid. Because renewables have little to no inertia, and can’t be used for frequency stabilization, other solutions are needed.

Do you have individual questions or do you want to schedule an appointment for a personal consultation?

Arrange a consultation

Palais des Congrès, Booth 354, Aug 25 - Aug 30, 2018

Unlock the potential of digitalization

During this year’s CIGRE session in Paris, August 26-31, Siemens experts will explain how to seize the digital opportunity and take the lead in the transition to a safer and even more efficient energy system. Visit booth 354 and discover the unique Siemens promise: security through a partnership that goes far beyond technology.

Siemens SVC PLUS FS at a glance

A convincing solution

By using a bulk number of supercapacitors, the new SVC PLUS frequency stabilizer (SVC PLUS FS) is a cost-efficient, compact solution that can emulate system inertia by boosting high active power into the grid when needed. It also offers voltage support by means of reactive power compensation.

While grids are undergoing fundamental changes in terms of power generation, renewable infeed and ever-growing demand, power quality and dynamic grid stability are at risk due to less synchronous power generation.

 

The grid frequency is balanced to 50 Hz or 60 Hz by parity of power demand and generation. The frequency must be kept within specific limits, even in the event of an imbalance: for example, from a disturbance. After a fault, the frequency can only be stabilized by an inertial response from generator-turbine sets. The mechanical kinetic energy defines the frequency drop after disturbance until the operating reserve is activated after several seconds by the primary frequency reserve (PFR). Fewer rotating machines result in shrinking instantaneous reserves, which increases the risk of exceeding critical frequency levels. This may lead to load rejection or a blackout. Grid operators are forced to keep power plants in operation in order to preserve the instantaneous reserve or to optionally invest in additional primary reserve. Some source of fast frequency response (FFR) is urgently needed to cover the gap between inertial response and operating reserves.

Better control of power grids, faster adaptation to load changes

Putting grid stability and power quality into practice, SVC PLUS FS offers a number of typical applications:

With a fast active power injection, the SVC PLUS FS covers the time gap between a grid disturbance and the activation of operating reserves.

The SVC PLUS FS combines dynamic voltage (STATCOM operation) and frequency support in one unit.

The SVC PLUS FS provides various system services that reduce the need of must-run capacity, which is currently provided by conventional power plants.

Disturbances at interconnections can lead to a cascading event in weak grids. To counter this, the SVC PLUS FS solution can flexibly and quickly change between injection and absorption of active power, thus strengthening the link by reducing overfrequency and frequency drops.

The SVC PLUS FS supports renewable power generation by providing grid code compliance.

   

SVC PLUS FS: more options for grid operators

In challenging times like ours, grid operators need versatile resources that give them options not only to react, but to act proactively, as depicted in the usecases/applications above. At that, with SVC PLUS FS, operators can be sure of a reliable, economical and space-saving solution with many advantages in terms of response time, control accuracy, and economic impact.

Turnkey solutions

While every power grid and every large industrial consumer has specific challenges in terms of power quality, active and reactive power compensation, and grid stability, our customized SVC PLUS FS turnkey solutions answer these challenges from a single source, including customized consulting.

 

From technical clarifications to on-site support and turnkey solutions, our service portfolio helps you optimize your assets and their performance throughout their entire service life – with comprehensive solutions from just one provider.

Key technical parameters of SVC PLUS FS

  • Can address any voltage level
  • Footprint: 2,700 m2
  • Active power: Pmax = +/–50 MW
  • Reactive power: Q = +/–70 Mvar
  • Available energy: 450 MJ
    (upscaling to 4x units in parallel possible)
Downloads

Additional information

Downloads

Stay in control

Optimal grid and frequency stability

With SVC PLUS FS, Siemens further enhanced the capabilities of a static synchronous compensator (STATCOM) with modular multilevel converter (MMC) technology to also support fast frequency response. Whenever your applications require a highly dynamic solution for voltage regulation and fast frequency support, the SVC PLUS FS is the first choice.

Four times a year, our newsletter will bring you timely and important information about our FACTS and HVDC solutions.

Subscribe here