In Wunsiedel, the future’s already here. With an independent energy system based
exclusively on renewables. Which is creating jobs and prosperity. Which is profitable
and the pride of an entire region. And soon even with green hydrogen.
Do you have any questions about this project?
One of Germany’s biggest green hydrogen plants
Hydrogen is crucial to Germany’s decarbonization strategy in terms of making mobility, refineries, metallurgy, steel production, the chemical industry, or chip manufacturing carbon-neutral. This is as true in Wunsiedel as it is anywhere else. But the topic, like many other energy issues, is seen here as part of a bigger picture. The hydrogen produced primarily from solar and wind power using PEM electrolysis is used not just as a raw material, but also as a long-term storage medium. The plant thus helps to relieve bottlenecks and add flexibility to the power grid. In Wunsiedel, quite naturally, the by-products of oxygen and waste heat are also integrated into the energy cycle.More flexibility and efficiency for municipal utilities
Today, public utilities are required to cover a wide range of activities and still turn a profit. “There has to be a new way,” says Marco Krasser, CEO of SWW Wunsiedel GmbH. That’s why he fully supports the intelligent networking of all energy systems to make full use of the potentials offered by the sun, wind, and biomass. “Energy sources are right outside everyone’s door,” says Krasser. “And ours even keep regrowing.”
The path of WUNsiedel is our commitment to achieving a consistent climate and energy strategy by 2030Marco Krasser,CEO of SWW Wunsiedel GmbH
Recognizing trends at an early stage and capitalizing on them for future economic success is a tradition at SWW Wunsiedel GmbH.
Wunsiedel was also an early convert to the idea of renewable energy and sustainable technologies. It is well known that this helps maintain local jobs while contributing to climate protection.
The next big step is the “path of WUNsiedel 2.0”, a lighthouse project for the entire energy business.
“It is up to us to leave the coming generations a world that is free from concerns about dwindling raw materials and environmental risks,” explains utility CEO Krasser.
That’s why in the future Wunsiedel’s supply network is to be fully based on renewables, semi-autonomous, and black start-capable.
The initial focus will be on power and heat generation, storage, control, and protection systems, and energy-efficiency. Plans for further stages in the project are already in preparation, for example for a power-to-gas or power-to-liquid plant. A pooling solution involving battery storage and an electrolysis system can earn additional revenue on the electricity balancing market in the future.
House of the future of energy
Maximum openness has been the focus of the path of WUNsiedel right from the outset. That’s why the “House of the Future of Energy” was created.
It’s an information center where residents can learn about the relation between climate protection and the energy supply system, how a local energy system works, and how much electricity and heat are currently being generated. The citizens of Wunsiedel are kept in the picture at all times and fully support the path of WUNsiedel.
Wunsiedel is no longer just a festival town, but is also an energy town, and is on its way to becoming a Smart City.Karl-Willi Beck, Mayor of Wunsiedel
Sector coupling is the basis for the path of WUNsiedel: All the elements involved in power generation are interconnected to make the best possible use of them.
The result is a stable and extremely reliable power supply system that will even allow excess production volumes and reserves to be sold on the energy market.
All system components are digitally networked using MindSphere. This creates room for further optimization in the future and creates attractive business opportunities beyond the supply mandate.