The SICHARGE UC family

SICHARGE UC, emobility, ebus charging

Energizing the world of utility vehicles

The Flexible Solution for the Future Urban Mobility

Want to find out more?

Brochure

          

Energizing the world of utility vehicles

The SICHARGE UC family

Providing you always with the best fitting hard- and software for your specific needs is our mission. For this, you can freely choose from the components of the SICHARGE UC family in its various power classes. One or multiple Charging Centers are always the core of the system as it contains the AC grid connection and the DC power electronics for your charging purposes.

Depot charging

The easiest way to connect to an electric vehicle is via a charging cable from the Charging Center. As space is valuable in many public places and logistic sites, you might want to distribute the DC power from the Charging Centers via up to 5 additional Frontends which you can install flexibly within your charging setup. As this cable connection requires some user interaction, and is dedicated for longer charging times, we generally see this installed in bus or logistic depots. 

Opportunity charging

Also used in depots but often dedicated for short-term opportunity charging, we see the use of Pantograph solutions, either installed on the vehicle or as part of the off-board infrastructure. The SICHARGE UC family provides solutions also for these automated connection possibilities via a mast mounted Pantograph or respectively via fix contact rails installed in the mast or roof mounted Hood. Either of such option is again powered by the Charging Center and if you want to combine frontends and Pantograph, you also have this flexibility.

Technical data

Downloads, support and services

Infrastructure and urban traffic control

Growing traffic volumes, increasing air pollution, rising costs: A mobility solution cannot solve all your infrastructure challenges on its own. But it will always contribute to making your city or municipality even more modern, more attractive and more environmentally friendly.

Customer Support

  • +491805242471

    (Telephone charges depend on provider)

References

Charging systems for ebuses

Siemens is at the forefront of this technology with tailored solutions that are already running on many locations.