This site uses cookies in order to improve your user experience and to provide content tailored specifically to your interests. Detailed information on the use of cookies on this website is provided in our Privacy Policy. You can also manage your preferences there.

By using this website, you consent to the use of cookies.

Learn more
OK

Desktop only

Desktop only

To use the writing tool please open Ingenuity on a desktop device

What are you writing about?

Need some help to get started? Read our writing tips.

What kind of article do you want to write?

Case study template

Use this template to write case studies and other long-form articles. Case studies present a challenge one of our customers faced and explains how we solved it. It consists of:

  • High-level summary
  • Background
  • Challenges
  • Findings
  • Reccomendations
  • Implementation

Use this template for: case studies, profile posts, future thinking, 'tools of the trade' or guest posts

List template

Show information in a concise, simple and structured way. Whether you’re writing "Top 10" articles or collecting content from across the web. Introduce your topic and let the readers explore it further themselves. This template consists of:

  • Introduction
  • List section

Use this template for: top 10, A-Z, checklists or similar list-based articles, curated lists of hyperlinks

Interview template

Present a personal conversation in a simple question-answer format. This template consists of:

  • Introduction
  • Questions
  • Answers

Use this template for: expert interviews, how-to guides.

Some writing tips

  • Choose a topic that truly fascinates you. Your enthusiasm will come through in your writing.

  • Write from your own point of view and use your own voice.

  • Challenge the status quo. In order to write about groundbreaking developments, you sometimes have to take a controversial stance.

  • Write in a clear, concise and comprehensible way. Write short sentences, use simple words and build a logical narrative.

  • Encourage discussion. Invite colleagues to contribute and readers to discuss your article.

  • Always check your grammar and make sure that your facts are correct before you hit “publish”.

Process Automation
  • LD
  • 0

Have you ever wondered what the best way to attach a transmitter to a process is?

I get this question all the time and it’s a fairly simple solution. While you can use remote seals, impulse lines are the most popular way to do this. An impulse line is tubing or pipe between the process and the transmitter. 

Why are impulse lines so popular? 

Impulse lines are popular for a number of reasons: 

  • It provides the highest accuracy measurement at the lowest installed cost.
  • This is usually the simplest installation to use.

It’s important to note that there are some considerations when using impulse lines.

Considerations? What do I need to worry about when I use impulse lines? 

Most processes are either liquids or gases, so one of the factors you need to consider is where you’re mounting your pressure transmitter. 

For liquid service, you want to mount the transmitter below the tap point so bubbles don’t accumulate in the impulse lines. Remember: air in the lines will cause errors in the transmitter reading because there will be a significant pressure drop across the bubble depending on the size of the bubble due to the energy that will be lost in compressing the bubble.

For gaseous service, you want to mount the transmitter above the tap point so liquid doesn’t accumulate in the impulse lines. Remember: liquid in the lines will cause errors in the transmitter reading because the height of the liquid will add to the process pressure being measured.

What do you do if you have to take the transmitter back to the instrument shop for service or calibration?

In case of maintenance, emergency removal, etc. you should always have an isolation system that allows easy removal of the transmitter. Different systems are applied to different transmitters. For example, if you have a gauge transmitter, you would use a Block & Bleed valve because there’s only one connection to the process. If you have a differential pressure (DP) transmitter, you would use a 3- or 5-valve manifold because you have a high- and low-pressure connection to the process. 

How do you know if a remote seal is needed to connect to the process? 

  • LD
  • 0

Comments