Camera housing
Splash-proof camera housing for GoPro
The Workpiece
Action camcorders enjoy great popularity and provide very good video recordings even under difficult conditions. Their compactness, wide-angle lenses and various mounting options mean these types of camcorders are also useful in the work area of CNC machines.
All information required for production, drawings, tool data and manufacturing description are compiled below.
Note
The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.