Corkscrew with Closure
Opening and closing wine-bottles
The Workpiece
Opening and closing bottles – these functions are united in one compact tool with the elegant, modular corkscrew. The corkscrew consists of two elements – the head and the sleeve – which are produced on a CNC turning machine. Together with the corkscrew spiral, it can be used as both a bottle opener and a stopper for open bottles.
All information required for the reproduction, tool data, drawings and ShopTurn machining plan are summarized in the following sections.
On frequent request, the order number of the corkscrew spiral is added to the manufacturing description: www.korkenzieherspirale.de, article no. S0150.
Note
The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.