Power solutions for twenty-first-century mines

Maximum reliability and cost efficiency
Mining operations require safe and reliable power supply under challenging circumstances. To meet productivity goals, conveyor belts, crusher, mills and float lines must operate continually. Every mine’s operations need specific power protection and automation solutions. Siemens Totally Integrated Power (TIP) takes a comprehensive view of mining electrification and covers all aspects from generation to utility infeed, through medium-voltage distribution, to end use. All supported across the entire lifecycle, seamlessly linked with automation and digitalization. TIP means dependable, safe, single-source mining solutions – viable long into the future requirements of this industry.
Power supply for unusually harsh environments
Diminishing productivity, harsh climates, remote sites, rising energy costs and water scarcity are just some of the challenges the mining industry faces every day. The ever-growing market demands require a solution enabling the perfect interaction of all assets during extraction, transportation and beneficiation. As a trusted mining partner, we help customers to meet their challenges and thereby enable them to set new benchmarks within their fields.Major challenges for mining
Safety and availability are essential in the mining industry – the extraction of valuable materials should, ideally, continue without interruption to ensure that operations in mainly inhospitable regions around the world will pay off. The power supply plays a key role in this regard: it has to be safe and reliable, as well as efficient and flexible.
Our answer: Totally Integrated Power
Specific solutions for the mining industry
Safety and efficiency are key demands on the power supply
The mining industry works mainly under extremely difficult conditions that involve a high risk of danger to humans and machines. The power supply is therefore subject to maximum safety precautions, since it has to operate with maximum reliability and safety. There are also increased demands in terms of energy efficiency. A solution must go beyond proven, integrated products: it also requires a precise understanding of the mining industry.
Our TIP offerings in depth

Complete power supply solution for coal mine and seaport in Mozambique
Nacala Corridor Project / CLN | Nacala-a-Velha, Mozambique The Nacala Corridor infrastructure project in Mozambique includes the seaport Nacala-a-Velha and the 912 km-long railroad to a coalmine in Moatize. Despite the tight timeframe and difficult transportation infrastructure in this part of Africa, the project was completed on time and within budget. The port was fitted with a complete container solution in five prefabricated e-houses, comprising transformers, medium- and low-voltage switchgear, and the appropriate motor control center for the power supply and drive control for the conveyor systems. The e-houses can be transported to a different location and re-used if, for example, a mine is closed,. Siemens also took the prevailing environmental conditions in the area into account. Overpressure within the e-houses prevents penetration by coal dust and deposits from the salty sea air. This highly efficient power supply solution enabled the port infrastructure to begin operations as planned.