Provide drinking water at a sustainable rate

Deliver the highest possible quality
Although the demand varies from region to region, according to the World Health Organization (WHO), adults require an average of 2 liters of drinking water daily; whilst children require 1 liter. But it isn’t just the human body that needs a daily supply of water; water is also necessary for other purposes such as doing laundry, daily hygiene and toilet flushing. Here, too, daily consumption varies widely. In Germany, the average citizen consumes about 130 liters per day, whereas in Italy they consume 260 liters and in Dubai as much as 500 liters. There’s a huge demand not only for a secure supply but also for quality in drinking water. With our hardware, software, and comprehensive services, we help you to design, operate and maintain your plant – for efficient and sustainable drinking water treatment.
Clean water through high tech
In many regions of the world, the demand for drinking water cannot be satisfied by groundwater alone. As a result, the treatment of surface water or even sewage to make it drinkable is increasingly important, especially in countries with constant water scarcity or where rivers are heavily polluted. In water treatment plants, Siemens’ intelligent automation systems, drive technology, industrial controls and power distribution ensure smooth operation and treated drinking water on a daily basis.Efficient energy management in water treatment
Drinking water is primarily obtained by purifying groundwater and surface water. This involves chemical or physical treatment processes and the setting of certain parameters, such as the pH value and ion concentration. The type of treatment depends on the quality of the raw water and is determined by the substances it contains and the substances to be removed. Energy consumption represents one of the biggest cost factors. One of plant designer’s and operator’s main tasks is to identify energy guzzlers in order to optimize your plant. Our intelligent products, solutions and services help you to achieve transparency in terms of energy demand and to significantly reduce your costs.
Simple control and monitoring of complex plants
Water treatment plants are often unmanned and are managed remotely from a central control room. The main challenge therefore lies in the maintenance and modernization of PC-based control systems. The virtual control technology, in particular, offers clear advantages: the entire control system server infrastructure is consolidated in a computer center. We facilitate your entry into future-oriented technologies with our lifecycle service that covers everything you need for a virtualization solution – all from a single source.
Shorter commissioning time using integrated plant engineering
Dynamic market requirements, environmental compatibility, and statutory requirements: International competitive pressure in the water industry is growing! This means that plant construction companies must shorten processing times and reduce project costs. With our integrated engineering, we offer plant designers and operators maximum data consistency through an optimized combination of application planning, distributed control system and device configuration – from the planning phase to automation and operation.
Products, solutions and services throughout the entire plant lifecycle
The parallelization and automation of work processes, their simplification and standardization, as well as digitalization and electrification are all important factors for improving the efficiency of your water treatment plant. Competing in the international market requires constant innovative strength and efficiency as well as increased productivity and quality throughout the entire plant lifecycle. With our customized solutions, products and services, we help you achieve integrated plant management.
Efficiency starts with planning
It is vital to already be working as cost-effectively as possible during the planning phase. Most importantly, saving time means saving money. The parallelization of work processes and their simplification and standardization are important factors for increasing efficiency. Innovative software and tools make optimal use of this potential.
Reducing configuration time and effort
Operators of drinking water treatment plants are constantly facing new challenges due to growing time and cost pressures.
The planning and further development of an innovative, high-quality system landscape requires system-specific, easy-to-use planning tools. With ProTime PCS 7, you can convert your individual requirements and existing quantity structure into SIMATIC PCS 7 plant configurations in a format which can then be ordered. This not only enables you to improve the quality of your system design, but also significantly reduces the time required.
Fault-free configuration of automation engineering
Errors in the selection of system components when automating a drinking water processing plant can result in delays and even supply problems at the time of commissioning. Using the TIA Selection Tool, you can ensure error-free configuration without expert knowledge. You not only save time but also money. The TIA Selection Tool is free of charge. The desktop and cloud versions permit cross-team cooperation with maximum flexibility.
Planning the automation of a water treatment plant
Uninterrupted operation, high water quality and reduction of plant costs are only some of the challenges of the water industry. Automation plays a decisive role in resolving these issues. Our automation engineering allows you to respond quickly to changes in the supply network. It stands for user-friendliness, high system availability, investment protection, future-proof technology and reduced total cost of ownership.
Planning drive engineering
With perfectly matched components such as enclosure, bearings, active parts, ventilation, and cooling system, we offer you the right motor and converter for every requirement. We thus ensure high plant availability, security of supply with high material quality through innovative processing and low energy consumption.
Planning the electrification of a water treatment plant
Our comprehensive range of power supply products permits a reliable, secure and efficient power supply with software and hardware products, systems and solutions for all voltage levels of your water treatment plant.
Integrated Engineering: shortening the time from planning to operation
Competing in the international market today requires constant innovative strength and efficiency, faster commissioning and uncompromising water quality from the very start. The solution: Enjoy the benefits of digitalization as early as the engineering phase using our Integrated Engineering concept, based on consistent software tools.
Parallelization of work processes
Growing international competition is making it increasingly important for planners and operators of water and wastewater plants and systems to increase productivity and quality. Severe time and cost pressures also make it necessary to parallelize work processes. This requires constant innovation and consistent data management. Life Cycle Engineering with our future-oriented COMOS software enables comprehensive management throughout your plant’s entire lifecycle – and thus the achievement of your goals.
Consistent end-to-end automation
Uninterrupted operation, high water quality and reduction of plant costs are only some of the challenges in the process industry. Automation plays a decisive role in resolving these issues. Our automation engineering allows you to respond rapidly to changes in the supply network. It stands for user-friendliness, high system availability, investment protection, future-proof technology and reduced total cost of ownership.
Efficient drive technology
With perfectly matched components such as enclosure, bearings, active parts, ventilation, and cooling system, we offer you the right motor and converter for every need. Thus, we ensure high plant availability, security of supply with high material quality through innovative processing and low energy consumption.
Optimal plant operation for high availability
Optimal plant operation is primarily based on high availability with minimal costs. Among other things, it requires data transparency and reliable equipment. Innovative software and proven products are valuable aids to profitable plant operation.
Certified energy management
Company-wide energy management across various sites can be a genuine challenge. With SIMATIC Energy Manager PRO, you can quickly display energy costs per generator set, machine, plant area, day, week, month or year. When integrated into the automation system, it lets you link energy and production data as well as plant information. Instead of having to analyze complex raw values, SIMATIC Energy Manager PRO combines the values and makes them accessible to you as meaningful indicators. TÜV certification of the solution makes it easier for you to comply with legal requirements in accordance with ISO 50001 and enables the energy- and cost-efficient operation of your drinking water treatment plants.
Protect plants against unauthorized access
With the growth of digitalization, comprehensive security in automation becomes increasingly important. Our Industrial Security concept includes all security levels and provides plant and network security as well as ensuring system integrity, thus providing comprehensive protection for the productivity of your water treatment plant.
Prevent faults and breakdowns in extreme ambient conditions
Mechanical loads, chemical and biological substances, condensation and temperature fluctuations reduce your water treatment plant’s durability. SIPLUS extreme technology protects your products against the resulting corrosion, dendrite and whisker formation and other harmful deposits, thereby preventing faults and downtimes. The expansion of the temperature range to -40°C and +70°C allows SIPLUS extreme products to be used even where the standard range is no longer sufficient.
Safe integration of distributed plants
Because drinking water treatment plants are often set up in a decentralized configuration with many distributed external stations, centralized control is important. With telecontrol, you can control your plant remotely and easily communicate with the individual parts of the plant that are separated in terms of space or locality. Using the telecontrol units you can, for example, detect leaks, monitor pumping and storage stations and check tank levels.
Consistent, end-to-end automation
Uninterrupted operation, high water quality and reduction of plant costs are just some of the challenges in the process industry. Automation plays a key role in resolving these issues. Our automation engineering allows you to respond quickly to changes in the supply network. It stands for user-friendliness, high system availability, investment protection, future-proof technology and reduced total cost of ownership.
Efficient drive technology
With perfectly matched components such as enclosure, bearings, active parts, ventilation, and cooling system, we offer you the right motor and converter for every need. We thus ensure high plant availability, security of supply with high material quality through innovative processing and low energy consumption.
Electrification over all voltage levels
Our comprehensive range of power supply products permits a reliable, secure and efficient power supply with software and hardware products, systems and solutions throughout a water treatment plant’s operating phase.
Reliable telecontrol technology
With our Telecontrol technology, you can efficiently connect and control individual process stations via remote networks.
Comprehensive water management system
Optimized operations management requires that plants and infrastructures in the water industry be intelligently controlled and managed. Our smart solution is the SIWA water management system – a modular solution for water networks.
Optimal maintenance for minimum downtime
Minimum downtime and optimal use of staff and resources are keys to sustainable success. With technology-based services throughout the entire plant lifecycle, in-depth knowledge of technologies and industry expertise, we create the conditions for greater productivity, flexibility, and efficiency – reliably, globally and around the clock. Thus, we enable you to perform predictive maintenance for optimal operation and minimum downtime.
Ensure high availability throughout the entire lifecycle
Both profitability and high plant availability are fundamental for operators of drinking water treatment plants. The value of their investment must be maintained by constantly adapting to new requirements, for example by increasing efficiency. To safeguard plant operation and ensure availability throughout the entire plant lifecycle, we offer a service program that supports and supplements the operator’s maintenance processes, optimizes the efficiency of plant components and guarantees plant safety.
Reliable monitoring of the plant
High availability of the automation concept is extremely important for properly safeguarding of plant supply. A SIMATIC System Audit provides transparency of the current status and serviceability of your SIMATIC automation system.
It thus provides a crucial basis for ensuring intelligent design and service strategies as well as efficient implementation of system upgrades and updates.
Introduce a preventive maintenance concept
Failures in a drinking water treatment plant can lead to serious supply problems. With our comprehensive range of preventive services, we help you avoid unplanned downtime by planning and implementing suitable maintenance measures in advance. Preventive maintenance also helps you to make the most of hidden potential through continuous optimization, thus improving your long term efficiency.