Straight talk: TSN – turbo power for PROFINET and OPC UA

Time-Sensitive Networking – Straight talk: Siemens is leading the way.

Time-Sensitive Networking – Straight talk: Our commitment to digitalization

Digitalization sets a high standard for industrial communication. Siemens is already relying on the rapidly growing open-communication standard Industrial Ethernet – with PROFINET at the field level and OPC UA at the control level. But Siemens is taking it one step further: with the Ethernet-based standard TSN (Time-Sensitive Networking) for reserved bandwidths, Quality of Service (QoS) mechanisms, low transmission latency, and parallel transmission of multiple protocols – including real-time-capable ones – in industrial networks.

Learn more about TSN from our experts:

Contact us

TSN FAQ 1 │Matthias Gaertner, Product Manager for the Digital Factory, Factory Automation Business Unit Germany, Siemens

What are the benefits of Ethernet with TSN compared with today’s Ethernet?

Basically, Ethernet with TSN supplements the existing Ethernet mechanisms in the areas of Quality of Service (QoS), including bandwidth reservation, as well as synchronization, low latencies, and even seamless redundancy.

 

The applications signal their communication requirements on the network and are guaranteed the requested QoS from the network. The various connections run in streams that enjoy bandwidth protection thanks to resource allocation in the memories of Ethernet switches. Basically, each of these streams can become real-time. As a result of these encapsulated streams, TSN also makes it possible to run multiple real-time protocols simultaneously in a single network (network convergence). This is fundamentally different from today’s Ethernet-based real-time protocols where the network only allows one real-time capable protocol.

 

[Further FAQs can be found in the next section]

What is TSN?

Straight talk on the path to the future: PROFINET and OPC UA with TSN.

Increasing digitalization of production processes requires more and more openness, robustness, determinism, and flexibility in industrial communication. Only production that communicates and responds extremely agilely can ensure the fast and reliable manufacturing of individual products while also meeting tight delivery schedules.

Straight talk for a giant step toward digitalization

While industrial control systems are dependent on real-time communication, IT systems rely primarily on open access to data. That’s why companies operate these networks separately. In the face of increasing digitalization, this separation must now be replaced by open, end-to-end networking that permits flexible, deterministic production. TSN (Time-Sensitive Networking) creates a standardized basic technology within the framework of IEEE 802.1 for guaranteed Quality of Service (QoS) and increased demands in the Ethernet. TSN comprises a series of individual standards that exclusively pertains to the OSI layer 2 of communication. This means that the user interface remains unchanged even with TSN.

From the automotive industry and machine-building to the food and beverage industry: TSN offers decisive advantages for industrial production, including reserved bandwidths, Quality of Service (QoS) mechanisms, low transmission latency, and parallel transmission of multiple protocols – including real-time ones. Siemens will be relying on TSN to help shape the digital transformation of industrial networks – from the field level and machine-to-machine (M2M) communication to the control and operator levels.

Driving development together

TSN has already gotten off to a promising start. As part of its ongoing development, it’s being tested at Labs Network Industrie 4.0 (LNI4.0). LNI4.0 is connecting testing environments and installations throughout Germany to further the advance of Industrie 4.0, and Siemens is one of the founding members. Along with a number of other industrial enterprises, the company is doing everything it can to test TSN interoperability with multiple vendors, and is conducting research in the test bed to assess the potential of TSN for M2M communication and machine networking all the way to the cloud. The knowledge obtained will be made available to standardization committees as needed for use in future development.

Frequently asked questions about TSN

What are the benefits of Ethernet with TSN compared with today’s Ethernet?

Basically, Ethernet with TSN supplements the existing Ethernet mechanisms in the areas of Quality of Service (QoS), including bandwidth reservation, as well as synchronization, low latencies, and even seamless redundancy.

The applications signal their communication requirements on the network and are guaranteed the requested QoS from the network. The various connections run in streams that enjoy bandwidth protection thanks to resource allocation in the memories of Ethernet switches. Basically, each of these streams can become real time-capable. As a result of these encapsulated streams, TSN also makes it possible to run multiple real time-capable protocols simultaneously in a single network (network convergence). This is fundamentally different from today’s Ethernet-based real-time protocols where the network only allows one real time-capable protocol.

Watch the video on TSN real-time communication on YouTube:

Watch video: PROFINET based on TSN

TSN in practice

Straight talk on the path to TSN: PROFINET and OPC UA

TSN unites existing IEEE standards that exclusively affect OSI communication layer 2. TSN isn’t a communication protocol; rather, it’s a basic technology that can be used in the coming years by both PROFINET and OPC UA as a kind of “turbo power.”

A sample model from the discrete industries

When machines communicate via TSN – Siemens demonstrates how it works

How might M2M communication with TSN look like in practice? Going beyond the theoretical, Siemens already has a trade show model that demonstrates this in practice using two robots with synchronized movements. Each of the robots communicates with a SIMATIC controller via PROFINET. Both controllers are synchronized via OPC UA PubSub (publish/subscribe) based on TSN. Thanks to bandwidth reservation, data transmission in the TSN network is precisely predictable, independent of load.

To demonstrate how TSN communication and standard Ethernet communication can be used in the same network, data in the model is also transmitted from the controller to a cloud – like MindSphere – via a communication processor.

Downloads, support, services

Straight talk with more information

Take advantage of additional sources of information to learn more about TSN – the turbo power for the Industrial Ethernet – with PROFINET and/or OPC UA. Brochures, informational materials, technical data, FAQs, and services – you’ll find them all here!

Everything to know about your technology

Fast, expert support for all your technical queries – even for products that have been discontinued or are no longer available for delivery

Well-trained for excellent handling

Receive standardized or individual expertise directly from the manufacturer – with training centers in more than 60 countries

Financial solutions for your success

We provide financial and technological expertise to help you boost your competitiveness

Contact

Straight talk: Let us advise you on TSN

The development of industrial networks never stands still. What is Siemens doing with TSN? How will you and the top-two technologies OPC UA and PROFINET benefit from Time-Sensitive Networking? And how can you optimize your network with TSN? Our experts are happy to answer these questions and many more.

Have questions? Our experts are happy to help:

Contact us