SIESTART™ hybrid solutions

Instant performance at the push of a button

Today’s energy producers depend on the safety of their operations and 100% availability of energy. They need to quickly respond to fluctuations in power demand, and must be able to shift to island operation to ensure an independent power supply when needed. The challenge is to meet these standards while also reducing emissions and costs.   Grid fluctuations are currently compensated primarily by fossil-fired power plants. They provide dispatchable and reliable power, but depend on external sources when an autonomous power supply is needed. In this case, battery energy storage system (BESS) serve as ideal back-up for instant power supply.   SIESTART sums up the capabilities of both fossil and renewable power generation by integration of BESS. Such hybrid solutions provide instantaneous, reliable and sustainable energy.

Want instant performance for an existing or a new plant?

Contact us

Power Plant Optimizer

ValuePlus concepts: ingeniously designed and efficiently implemented

Discover the ecomic and ecological added value of our innovation driven power plant solutions.

New opportunities

Boosting existing and new plants

SIESTART enables an advanced upgrade for existing power plants, enriching them with new features, while extending performance and providing new business opportunities – independently of OEM technology. It also significantly improves the value of newly built power generation units. With its exceptional flexibility, SIESTART can be used with gas turbines, steam turbines and combined cycles. This helps you to easily scale your power production operations and reduce operating expenses (OpEx). 

A hybrid solution - summing up capabilities

SIESTART integrates the benefits of fossil-fired power generation with battery energy storage system (BESS)

 
 
Conventional power generation
Battery storage
SIESTART
Dispatchability
●●●●●
●●●○○
●●●●●
Reliability
●●●●●
○○○○○
●●●●●
Continuity
●●●●●
○○○○○
●●●●●
Instant performance
○○○○○
●●●●●
●●●●●
Black start capability
●○○○○
●●●●●
●●●●●
Power balancing
○○○○○
●●●●●
●●●●●
Emissions
●●○○○
●●●●●
●●●●●

Fossil energy suppliers increasingly face the challenge of having to respond as quickly as possible to load fluctuations. SIESTART provides the ideal solution, offering more flexible and more cost-effective power plant operation – with capacity at the push of a button. Using state-of-the-art energy storage systems, fossil power stations can be ramped up and down more quickly, and be used as a more targeted comprehensive solution – even for black starts when necessary. 

Applications

Typical implementation cases for a hybrid solution

The combination of a battery energy storage system (BESS) and fossil-fired power plant opens up a range of different services for the grid and power plant operators, including black-start capability and regulating services.

Black start of a gas turbine on loss of off-site power and support to restore the grid

Generally, power plants use small diesel generators to start turbines, or to provide power references such as voltage and frequency to allow renewable power generators to reconnect. Due to its speed of response as well as advanced control, SIESTART can be used as an alternative to a black start diesel generator. It saves time and improves reliability while helping you boost revenues. SIESTART can also provide the necessary short-circuit power to ensure a given protection sequence.

Increasing the power gradient of the supply to the grid on start-up or ramp-up of the power plant

Run-up and start-up of a gas turbine require time. However, even the fastest and most flexible power plants are still too slow to respond to grid fluctuations within a matter of seconds and almost impossible to respond to demand down-turn situations. Depending on the scale of the battery energy storage system (BESS), it can immediately supply power to the grid and absorb power from the grid and can therefore fully or at least partially take over this activity for a brief period. In this mode of operation the BESS would supply power to the grid while the gas turbine is ramping up. The battery energy storage system continues to supply power to the grid until the gas turbine takes over and the battery can then be recharged (if needed).

Provision of regulating capacity with the power plant from cold start or in operation

The provision of regulation capability using battery energy storage system (BESS) is significantly faster (< 1 sec) and much more precise than what can be accomplished with a fossil-fired power plant. Power plant operators can generate additional business opportunities by offering this regulation capacity, and operating the plant with more flexibility. On simultaneous implementation of the BESS and the gas turbine, the battery assumes the task of fast response (both positive and negative), while the gas turbine only supplies the energy to deliver extended service requirements and balance the battery charge level. Such an optimized operating mode significantly reduces the stress on the gas turbine such as fuel and maintenance costs.

Accelerated output adjustment on load changes and stabilization support for volatile load conditions

The battery energy storage system (BESS) supports the gas turbine in accelerating output adjustment and stabilization/smoothing of volatile load. BESS can already supply energy before and during gas turbine startup, therefore the overall energy output of the power plant to the grid can be significantly accelerated to respond to sudden load changes.

Offering up to rated-power plant output and maintaining spinning reserve with the SIESTART battery energy storage system (BESS)

Should spinning reserve be required to respond to large grid under-frequency, the BESS can be used to temporarily increase the maximum power output of the power plant at the POI. The otherwise permanently restricted output from the power plant can then by circumvented, and therefore offering power generation capacity up to rated output opens up additional revenue opportunities.

Stabilization of gas and steam turbines during grid outages as well as safe transition of the power plant to island mode

The most important objectives in stabilizing gas and steam turbines on grid outages are thus to limit the speed increase as well as to maintain turbine operation at the auxiliary power requirement or in island mode. On disconnection from the grid, the excess energy in the rotating system must be removed through the generator as electrical energy and input to/stored in the battery energy storage system (BESS). This significantly reduces the acceleration and thus the speed increase. Conflicting oscillations between the BESS and the turbine are not anticipated, because the battery energy storage system operates in power-controlled mode and the turbine in speed control.

Merging technologies

Fully integrated battery energy storage system (BESS) combined with your power plant

SIESTART hybrid solutions combine the performance of fossil-fired power plants with reliable battery energy storage system (BESS), jointly controlled by our SPPA-T3000 control system. It provides additional power to the grid within milliseconds.
Comprehensive experience

Count on an integrated solution from power plant experts

Siemens is the world leader in flexible power generation for the changing demands of grids. The ability to combine the high performance of a conventional power plant with the instantaneous response of a battery energy storage system makes our solution ideal for many use cases, maybe even yours. Put your trust in a partner that knows the power business and power technologies inside and out.
Downloads, support, and services

Your source of information

Here’s where you’ll find material to download, contact details, and links to the services we offer.

For more information, please contact our Energy Customer Support Center

 

Siemens AG

Freyeslebenstrasse 1

91058 Erlangen

Germany

(Charges depending on provider)

(From the German fixed network € 0.14/min.

and from the German mobile phone networks

max. € 0.42/min.)

Training

31 training centers worldwide – we offer customized trainings. Benefit from our network of experts.

Plant service

Maintenance, repair, modernization – our Power Generation Services ensure that your facility maintains its value. Enjoy long-term confidence.

Financing

From consulting to financing – Siemens offers financial solutions for business-to-business customers worldwide. Talk to the experts.

Online Customer Portal

The latest information, news, product details – in our exclusive Customer Portal you are directly informed. Keep your finger on the pulse.

References

The solution in practical operation

Why should you buy a solution that has not stood the test yet? Siemens has combined conventional power generation with an energy battery storage system in different use cases.
News and events

Stay up-to-date

The latest news about our projects. Industry events that affect us – and you – in your market. Find out what’s happening in the energy industry.

Benefit now

Boost your plant’s possibilities

Conventional energy suppliers increasingly face the challenge of having to respond as quickly as possible to load fluctuations. SIESTART provides the ideal solution, offering more flexible and more cost-effective power station operation – with capacity at the push of a button. Using state-of-the-art energy storage systems, conventional power stations can be ramped up and down more quickly, and used as a more targeted comprehensive solution – even for black starts when necessary.

Want instant performance for an existing or a new plant?

Contact us