Empower your data value - with modularized engineering

COMOS – Making data work. The path to Industry 4.0 offers many opportunities for companies in the chemical industry to act promptly. Those who know how to increase the value of plant data in a targeted manner will have a lasting competitive edge. Key factors include centralized data storage and the use of smart templates. Design and engineering efforts can be significantly reduced with the help of standardized modules such as those implemented in an integrated software solution like COMOS.
Want to talk to our experts?

Contact us

Challenges

Digitalization is changing business

Digitalization is changing business fields on a fundamental level. Sectors like the chemical industry are also facing the challenge of the next step towards Industry 4.0.

There is an ever-growing need to increase the speed of production under favorable conditions. Customer requirements are becoming more varied and sophisticated. Engineering projects are under tremendous time and cost pressure. Project bids must be calculated as precisely as possible, which is made difficult by the amount of information that’s scattered across a variety of sources.  It’s especially important during the bid phase to work efficiently. Preparing a competitive bid is an essential factor in succeeding in the plant and project business.

A consistent flow of information still isn’t implemented in many companies

Many companies lack a consistent, seamless flow of information. Information is frequently available only in analog form or in distributed systems and has to be copied manually – and therefore often incorrectly and with a great deal of effort. Plant data is often recorded multiple times across different departments and is inconsistent, incomplete, or outdated. This makes it difficult to reproduce experiences from previous projects, resulting in a critical loss of valuable company expertise.

Modularized engineering

Download flyer

Modularized engineering

Centralized data storage and smart templates as a basis for digitalization

The integrated software solution COMOS lays the foundation for successful digitalization in the chemical industry. COMOS stores and manages all information relating to engineering and proposals in a central database.

COMOS makes it possible to consistently implement modularized engineering for all disciplines – from proposal preparation and engineering to project completion. Using smart templates in sectors like the chemical industry makes engineering and design extremely efficient. Smart modules give engineers and operators a high degree of bidding and planning flexibility. Proposals can be prepared quickly and are placed on a solid footing for clear cost calculation. After the order is received, a large part of the basic engineering has already been completed. Modularized engineering can drastically reduce over- and under-engineering. With the standardized modules, customer requests are individually and precisely implemented. Even regulatory requirements (compliance) are reliably met. COMOS also enables companies to establish a solid, long-term knowledge base, safeguard their expertise, and attain lasting success.

COMOS Modularized engineering in the chemical industry: an example.

Benefits

Consistency from the bid phase and engineering to project completion

The COMOS software solution draws on standardized smart templates for fast and efficient work. A configurator can be used to create and apply these templates.

The configurator in COMOS is modified using a graphical interface, which makes it unnecessary to program complex rules. The preliminary flow charts, technical specifications, and part lists are generated on basis of variant drivers (including capacities, framework conditions, and technical requirements). A proposal manager where the costs and prices of objects are assigned is used to ascertain the proposal information. For subsequent engineering, smart templates can again be used: for example, for generating piping and instrumentation diagrams (P&IDs), electrical engineering documentation, schematic diagrams, bills of materials (BOMs), and lists. Once the project has been completed, the collected information can be reused for new projects. The data can also be used for recalculations.

Your benefits at a glance

Modularized engineering based on COMOS

MTP Facilitates Modular Production

Read Blog

References

Modularized engineering in practice

Solutions for creating data value are already being successfully implemented in the chemical industry. Discover sample applications that demonstrate how COMOS helps increase the value of your data in actual practice.
Contact

Empower your data value – with Modularized engineering

Design and engineering efforts can be dramatically reduced by using templates like those implemented in an integrated software solution like COMOS. Want to talk to our experts? Contact us:
Individual applications

Empower your data value with …

Discover targeted, practical COMOS applications.