Set this page to
Go to Siemens Global Website
Go to Siemens in your region
Set this page to
Go to Siemens Global Website
Go to Siemens in your region
We supply non-gapped and externally gapped line surge arresters for overhead lines for up to 800 kV. Line surge arresters offer the most economical and effective lightning protection on new and existing overhead line systems. Special areas of application include e.g. areas with high lightning frequency, poor soil or tower grounding resistance (e.g. for sandy or rocky ground), unprotected overhead lines (without ground wire), reducing switching impulse current overvoltages in high-voltage systems, and providing extended station protection.
Non-gapped line surge arresters (NGLA) offer a high degree of mounting flexibility and operational reliability. Depending on the tower design and the arrangement of insulators and lines, these arresters can either be installed directly on the insulators or on the tower.
Thanks to their high energy absorption capacity, non-gapped line arresters offer a very high level of protection against overvoltages caused by lightning and network-generated switching impulse current overvoltages.
To galvanically isolate the line surge arrester from the line voltage in the unlikely event of a fault or thermal overload, a disconnector is installed in series. It automatically and immediately disconnects the line surge arrester from the line voltage. This allows the affected overhead line to continue to be used until replacement can be scheduled. In addition to the line surge arresters, the new ACM advanced monitoring system can be installed to provide arrester condition monitoring. This system monitors wirelessly and provides detailed information about leakage currents and converted energy. |
EGLA line surge arresters have an external spark gap placed in series that galvanically isolates the active part of the arrester from the line voltage in normal conditions. In case of lightning, the spark gap is ignited and the overvoltage is safely discharged to the ground. EGLA line surge arresters prevent all insulator flashovers caused by lightning strikes. As such, EGLA increases network stability as well as the availability of the overhead line.
Siemens EGLA line surge arresters are available for system voltages of up to 550 kV. All Siemens EGLAs are designed and tested to comply with the latest IEC 60099-8 standard, which became effective in January 2011. |
Siemens optionally offers software analysis (simulation) based on Cigré studies to examine and conduct preliminary tests of customer-specific applications as a way of determining the optimal, cost-effective solution. With this approach, the customer only needs to equip particular phases or individual line segments with line surge arresters, and can still ensure sufficient lightning protection of the overhead line.
In the first phase of an analysis, all important parameters of the transmission line under study are entered into the simulation software, and the installations to be examined are selected. This approach takes the following factors into consideration:
Схоже, ви використовуєте браузер, який не підтримується. Зверніть увагу: це може вплинути на відображення сайту та його юзабіліті. Рекомендовано завантажити останню версію браузера або встановити інший.