Go to Siemens Global Website
Go to Siemens in your region
Go to Siemens Global Website
Go to Siemens in your region
Siemens expertise and experience produces superior transformers for the HVDC schemes, HVDC Classic and HVDC Plus, in bulk power transmission, offshore and onshore grid connections, back-to-back systems and other HVDC use cases. Portfolio: transformers, upgrades, replacement, repair, refurbishment, and the supply of selected components HVDC ratings: up to 12 GW and up to 1,100 kV DC AC grid connections: up to 1,050 kV AC Features: Compact designs, high reliability, and proven technology from Siemens’ global manufacturing network
The world´s first transformer, which has been designed and manufactured for the HVDC transmission line with the highest direct-current electricity of ± 1,100 kilovolt (kV) has been dispatched from Nuremberg, Germany. The transformer is now on its way to its Chinese destination. This will take approx. three months. In the future the transformer will enable low-loss and extremely efficient high-voltage direct-current (HVDC) power transmission over a record distance of 3,284 kilometers with a transmission capacity of twelve gigawatts.
Smart grids are emerging as a necessary response to the environmental, social and political demands placed on energy supply.
With their capacity to increase transmission efficiency, innovative HVDC solutions will play a key role in making sustainable low-loss AC/DC hybrid grids a reality. With the transmission power capability of HVDC systems steadily on the rise, requirements for converter transformer technology and design have greatly increased. Customers rely on Siemens’ experienced design teams to help them master transmission and grid challenges around the globe.
Hundreds of Siemens HVDC Converter transformers are in successful operation all over the globe. Active in the field since the 1970s, Siemens Transformers has huge experience in designing and manufacturing HVDC units. Rising to challenges, from in-time delivery for large order volumes to building record-setting units that meet highest technical specifications, Siemens stands out for trademark reliability and customer focus.
For operators, assessing reliability risks is crucial for evaluating the total cost of ownership of an HVDC transformer. Including failure rates (FR) and mean-time-between-failure rates (MTBF) of a Siemens HVDC transformer in purchase considerations lowers your risk potential and ensures savings over the entire transformer lifecycle.
Siemens transformers reach a failure rate well below 0,5 percent. According to the international standard defined in IEEE C 57.117 this translates into excellent product reliability. It equals an MTBF rate of more than 200 service years.
Siemens has been pioneering transformer technology, since the dawn of HVDC converter transformer production. As a world-class leader synonymous with top quality and reliability, Siemens enables the successful implementation of HVDC transmission systems with dedicated research and development programs.
- DC voltages: 500 kV, 800 kV, 1100 kV
- Line ratings: 3GW, 6,4GW 8GW, 10GW and 12 GW
- AC voltages: 525kV, 1050kV
Designing and building a HVDC transformer is a complex process. The insulation to ground and between line and valve winding has to withstand AC and DC stresses. Valve windings need to be tested with voltages determined by the protection level of the DC side. Harmonics in currents cause losses in various parts and DC currents influence the magnetization of the core.
Siemens ensure that the quality of the core sheet, the lamination of the sheets, and the nominal induction all conform to rigorous requirements covering losses, noise level, overexcitation, etc.
Siemens Transformers delivers HVDC converter transformer including all main components to facilitate transportation, installation, and safe operation.
A strong Siemens transformer factory network around the globe creates leading HVDC Converter transformer technology and pre-manufactured components.
To meet public local content requirements, Siemens enables and supports local transformer manufacturers to produce HVDC converter transformers based on Siemens technology. However, to ensure high HVDC converter transformer reliability, Siemens Transformers implements in-house prototype design and manufacturing.
capacity
DC transmission voltage
transmission capacity
households supply capacity
AC input offshore
DC HVDC link
DC transmission voltage
DC capacity
power rating
The 170 kV DC Welsh Converter Station in Texas links the network of the Energy Reliability Council of Texas with the Southwest Power Pool of the eastern US network. The back-to-back tie is equipped with 7 Siemens transformers. It operates at a power rating of 600 MW at a voltage level of 345/345 kV, 60/60 Hz.
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser: