Siemens external “Digital Sensor Link” (DSL) for Sitrans FST030 ultrasonic flow system
Harleysville, PA
August 10, 2020
Siemens is proud to announce the latest in the series of feature updates and performance improvements for the Sitrans FS230, our premium line of clamp-on ultrasonic flow systems. The external “Digital Sensor Link” (DSL) is an external digital module for the Sitrans FST030 flow transmitter installed near the measurement pipe. The DSL processes analog signals from the sensors and immediately digitizes the measured values into flow data, which is sent to the transmitter via a “Siemens Sensor Link” (SSL) cable for further processing. The external DSL module is an alternative to the built-in internal DSL previously standard in the FST030 transmitter. There are two variants of the DSL, one configured for liquid fluid flow and the other for gas flow.
The external DSL provides additional flexibility and an extended range of functions:
- 100 Hz digital high-speed interface between the transmitter and DSL
- Measurement of 1 to 4 independent measurement paths (on a single pipe)
- 2 analog inputs for temperature or current measurement near the pipe
- External DSL and sensors come with FM Class 1 Div. 1 approval; wall-mount transmitter is installed in FM Class 1 Div. 2 environments
- IP66/68 protection against dust and water intrusion
- Up to 500 ft between the DSL and transmitter possible with SSL cable
- Short analog sensor cables from on-pipe sensors, providing optimal RF interference suppression
- Cable cost savings for longer cable runs, as only a single cable is required for the full run instead of 2 to 8 separate cables from each sensor
The new external DSL is available in the following product variants:
Sitrans FST030 ultrasonic transmitter model prefix 7ME3723, where the part numbers carry options N, Q, V, W. in the 14th position.
Further Information:
For any questions regarding this release, please contact Eric Heilveil, Product Manager, by phone: 215-385-0180 or e-mail: eric.heilveil@siemens.com
For additional information about the Sitrans FS230 clamp-on ultrasonic flow system, please visit: www.usa.siemens.com/fs230
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global powerhouse focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. For more than 160 years, the company has innovated and invented technologies to support American industry spanning manufacturing, energy, healthcare and infrastructure. In fiscal 2018, Siemens USA reported revenue of $23.7 billion, including $5.0 billion in exports, and employs approximately 50,000 people throughout all 50 states and Puerto Rico.