Siemens launches new fault-interrupting capacity for Fusesaver™ medium-voltage circuit breaker
Raleigh, NC | Feb 27, 2017
Fusesaver technology investment paid back in savings from less than four truck rolls
Siemens has announced its ultra-fast Fusesaver™ medium-voltage circuit breaker now includes 6.3 kA fault-interrupting capacity. This new feature will help utilities apply the technology across more of their distribution network to further improve system performance in case of temporary faults. The technology clears temporary faults in less than one cycle and pays for itself in savings from less than four truck rolls that would have been required to address a line outage.
“With 80 percent of power outages caused by temporary faults, it’s essential to have fast-acting technology that can clear faults literally faster than a blink of an eye,” said Brian Dula, vice president of Siemens Medium Voltage and Systems. “The new 6.3 kA fault-interrupting capability uses the latest in digital grid technologies to improve a utility’s reliability while positively impacting their bottom line.”
Weighing only 12 pounds and able to be mounted directly on the conductor, cross‑arm, or pole, the Fusesaver can be securely installed in less than 30 minutes a phase without having to rely on any additional mounting components. Featuring peer-to-peer wireless communication, the Fusesaver can operate in single-phase or multi-phase configurations.
Coupled with the SiemensConnect application, settings changes can be made while the Fusesaver remains in service, and event logs and load profile data can be downloaded without needing to send a high-voltage crew or bucket truck. This leading edge fault-interrupting technology also helps utilities improve performance on key industry reliability indicators like the System Average Interruption Duration Index (SAIDI) and System Average Interruption Frequency Index (SAIFI).
For further information on Siemens medium-voltage outdoor circuit breaker technology, please see usa.siemens.com/fusesaver.
Contact for journalists
Annie Satow
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global powerhouse focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of systems for power generation and transmission as well as medical diagnosis. With approximately 351,000 employees in 190 countries, Siemens reported worldwide revenue of $88.1 billion in fiscal 2016. Siemens in the USA reported revenue of $23.7 billion, including $5.4 billion in exports, and employs approximately 50,000 people throughout all 50 states and Puerto Rico.
Language: English