Siemens to provide new switchgear technology for National Grid substation project
Wendell, NC | Oct 22, 2015
- New arc-resistant switchgear technology design resulted in smaller project footprint and lower overall cost
National Grid, a multinational electricity and gas utility, has chosen Siemens to provide its 63 kA arc-resistant switchgear technology for the utility’s new electric substation in downtown Providence, Rhode Island. The new location, replacing the National Grid’s existing South Street Station, will provide reliable, efficient power to the utility’s customers including the City of Providence and much of downtown Providence. Siemens’ 63 kA type GM-SG-AR switchgear is designed to improve power reliability and includes arc-resistant features that increase safety conditions for workers and operators. The technology’s design will also allow National Grid and contractor TRC Companies, Inc. to reduce the project’s physical footprint, resulting in significant project cost savings.
“This Siemens switchgear is a great technology solution for utilities and contractors who are looking for flexibility in moving or upgrading substation technology, especially when overall safety is your goal and space constraint is an issue,” said Steve Redden, senior project manager of power delivery engineering at TRC Companies, Inc.
Siemens recently extended the rating of its GM-SG-AR arc-resistant switchgear to 63 kA, which broadens its applications into the oil and gas, chemical, and power generation spaces that require the highest level of arc-resistant, fault-current interrupting.
“As power systems become increasingly complex, utilities and power operators rely on advanced technologies like our 63 kA type GM-SG-AR switchgear to operate the power grid more, efficiently, safely, and reliably than ever,” said Brian Dula, vice president of Siemens Medium Voltage and Systems. “We’re proud that our work with National Grid and TRC on this project is bringing the next generation of power technologies into the substation in an innovative and cost-effective way.”
For further information on Siemens 63 kA type GM-SG-AR medium-voltage, arc-resistant technology, please visit http://w3.usa.siemens.com/powerdistribution/us/en/product-portfolio/Medium-Voltage-Switchgear/Pages/metal-clad-arc-resistant-switchgear.
This press release and a press picture / press pictures/ further material is available at http://news.usa.siemens.biz/.
Contact for journalists
Annie Seiple, Siemens
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. With 343,000 employees in more than 200 countries, Siemens reported worldwide revenue of approximately $98 billion in fiscal 2014. Siemens in the U.S. reported revenue of $22.2 billion, including $5.2 billion in exports, and employment of approximately 50,000 people throughout all 50 states and Puerto Rico. To receive expert insights sign up for Siemens’ U.S. Executive Pulse leadership blog. Follow us on Facebook and Twitter at: .
Language: English