Siemens to provide all major electrical equipment for fuel efficient power plant in Michigan
Wendell, NC | Feb 18, 2016
Siemens providing low- and medium-voltage switchgear, power transformers and motor control centers for safe, efficient control and operation of Holland Energy Park
New distributed control system will control and monitor entire plant
Siemens has been chosen to supply critical low- and medium-voltage electrical equipment and power transformers for the new Holland Energy Park combined cycle power plant in Holland, Michigan. The local municipal utility, Holland Board of Public Works (HBPW), is replacing an aging coal-fired plant with a new fuel efficient modern power plant, slated for commercial operation in fall 2016.
Siemens will install its SPPA-T3000 Distributed Control System technology, a software system that connects, control and allows for communications of the hardware throughout the plant, integrated with its medium- and low-voltage switchgear and low-voltage motor control center for centralized monitoring and operation for the entire electrical system. The technology will include the latest arc-resistant switchgear, which allows workers to safely operate the electrical equipment. Siemens was also chosen last year to supply two gas turbines and one steam turbine for the combined cycle power plant.
“Siemens has aggressively pursued the installation of their equipment on this project. We are pleased to have their great technology and its’ attendant reliability installed at Holland Energy Park” stated Dan Nally, Business Services Director for the HPBW and Project Director for HEP.
“We’re excited to extend our technology partnership with Holland Energy Park by delivering not only our leading turbine technology but providing our extensive expertise in the electrical infrastructure space,” said Kevin Yates, president of Siemens Energy Management. “Electrical systems play a critical role in ensuring the safe, efficient and successful operation of innovative energy systems like Holland Energy Park and other facilities across the country.”
Siemens will be providing its new 63 kA type medium-voltage GM-SG-AR switchgear for the Holland Energy Park electrical infrastructure. The technology is designed to improve power reliability and includes arc-resistant features that increase safety conditions for workers and operators. The recently extended rating broadens its applications into the oil and gas, chemical and power generation spaces that require the highest level of arc-resistant fault-current interrupting. Siemens will also provide three 138-13.8 kV generator step-up transformers to help provide reliable power for the Energy Park.
Siemens’ scope of supply regarding power generation includes two SGT-800 gas turbines and one SST-400 steam turbine. Siemens will also provide a long-term service contract for the SGT-800 gas turbines. The new plant’s cogeneration capabilities provide it with an extremely high fuel efficiency level and will generate approximately 125 megawatts (MW) in summer and 145 MW in winter.
The new plant will use waste heat from the circulating water system for use in an expanding downtown snowmelt system. Circulating water from the Holland Energy Park plant will run through a heat exchanger to warm water for the snowmelt system in the downtown area. This, in turn, alleviates the need to salt or plow during the winter months. The system can melt approximately 1 inch of snow per hour in temperatures of 15 to 20 degrees Fahrenheit.
In addition to its function in the snow melt and power space, Holland Energy Park will serve as an educational resource, with special architectural details that allow for public tours and public green space surrounding the facility with nature trails. HBPW has registered with the Institute for Sustainable Infrastructure in an effort to obtain an Envision Platinum Rating for this state of the art facility.
The project is expected to be completed in February 2017.
For further information on Siemens power technology, please visit www.usa.siemens.com/powerdistribution.
This press release and a press picture / press pictures/ further material is available at http://news.usa.siemens.biz/.
For further information on the Siemens gas turbine order for the Holland Energy power plant, please visit http://www.siemens.com/press/en/pressrelease/2015/power-gas/pr2015020134pgen.htm
Contact for journalists
Annie Satow, Siemens
Phone: 202-316-0219; E-mail: annie.seiple@siemens.com
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global powerhouse focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of systems for power generation and transmission as well as medical diagnosis. With approximately 348,000 employees in more than 190 countries, Siemens reported worldwide revenue of $86.2 billion in fiscal 2015. Siemens in the USA reported revenue of $22.4 billion, including $5.5 billion in exports, and employs approximately 50,000 people throughout all 50 states and Puerto Rico.
Language: English