Siemens to Automate MTA’s Queens Boulevard Subway Line
NEW YORK | Aug 27, 2015
- Siemens to install Communications-Based Train Control (CBTC) rail automation technology on one of New York City Transit’s busiest lines
- Upgrades will increase number of trains running on the Queens line, increasing passenger capacity
NEW YORK--(BUSINESS WIRE)--Siemens has been awarded a $156 million contract by the Metropolitan Transportation Authority (MTA) to install Communications-Based Train Control (CBTC) on the Queens Boulevard Line, one of the busiest subway lines on the New York City Transit system. The radio-based CBTC technology provides real-time data on vehicle position and speed conditions, allowing system operators to safely increase the number of vehicles on a rail line. This results in greater frequency of train arrivals and allows MTA to accommodate more passengers on its system. The CBTC technology reduces the amount of wayside equipment and, as a result, reduces maintenance costs and service disruptions. Additionally, the technology precisely locates each train on the tracks and controls speed, improving on-time performance for riders and employees.
“Through our work on the Canarsie line, we’ve seen first-hand that CBTC technology can have a significant positive impact on ridership for the New York City subway system,” said John Paljug, head of Siemens Rail Automation. “We’re extremely excited to extend our technology partnership with the MTA and bring advanced automation technology to riders on the Queens Boulevard line.”
Siemens is supplying the onboard equipment for a total of 305 trains and installing the wayside signaling technology at 7 of 8 field locations. Through automated signals and sensors throughout the line, the CBTC technology provides continuous updates on system status that results in fewer delays and up-to-date travel information shared with riders via public address systems, electronic screens and mobile applications. The system also reduces the amount of wayside equipment and employs back-up systems, resulting in fewer instances of service disruption and greater reliability.
The system will be managed and deployed by Siemens New York City based rail automation team of CBTC experts which has been working with NYCT for over 15 years.
Every day, over five and a half million passengers ride the over 100-year old New York City subway system. To keep pace with the increasing number of passengers, the system is continuously being modernized. In addition to the new system on the Queens Boulevard line, Siemens successfully installed CBTC technology on MTA’s Canarsie “L” line that operates from Chelsea (Manhattan), through Williamsburg to Canarsie (Brooklyn). The automation technology has allowed MTA to handle and sustain increasing ridership on the line over the last 20 years.
Siemens has proven the CBTC technology for the New York City Transit system through a four year testing project on the Culver line. Through this testing period, Siemens was able to establish one set of specifications and standards for CBTC technology on the New York City subway system that will be used for the Queens Boulevard line project and all future CBTC projects.
Siemens CBTC solution Trainguard MT is the most extensively deployed automatic train control system in the world and is used by more than 20 metro operators including Paris and Beijing. This is Siemens’ fifth CBTC project in the U.S.
Development work is expected to begin on the Queens Boulevard line late this summer with the major installation beginning in mid-2017.
This press release, photos and additional material are available at news.usa.siemens.biz.
Siemens’ Rail, Transit & Mobility Portfolio: Siemens Rail Automation business unit is part of the Siemens Mobility Division which provides efficient and integrated transportation of people and goods by rail and road – including all products, solutions and services regarding mobility. Siemens designs and manufactures across the entire spectrum of rolling stock including commuter and regional passenger trains, light rail and streetcars, metros, locomotives, passenger coaches and high-speed trainsets. In the U.S., Siemens is providing rail vehicles, locomotives, components and systems to more than 25 agencies in cities such as Washington D.C., New York, Boston, Philadelphia, Denver, Salt Lake City, Minneapolis, Houston, Portland, Sacramento, San Diego, St. Louis, Atlanta and Charlotte. Cities also rely on Siemens to provide traction-power substations and electricity transmission, as well as signaling and control technology for freight and passenger rail and transit systems. Siemens has transportation manufacturing hubs in: Sacramento, CA; Louisville, KY; Marion, KY; Pittsburgh, PA; Tualatin, OR
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. With 343,000 employees in more than 200 countries, Siemens reported worldwide revenue of approximately $98 billion in fiscal 2014. Siemens in the U.S. reported revenue of $22.2 billion, including $5.2 billion in exports, and employment of approximately 50,000 people throughout all 50 states and Puerto Rico. To receive expert insights sign up for Siemens’ U.S. Executive Pulse leadership blog. Follow us on Facebook and Twitter at: www.twitter.com/siemensUSA.
Contact:
Siemens
Annie Seiple, 202-316-0219
Language: English