Built-In Isolation Technology Feature Now Standard on All Siemens Fire Safety Devices and Detectors
Saves Time and Money, Improves Survivability and Serviceability
Florham Park, N.J. | June 23, 2020
- Secure, maximum protection against short circuits for a more reliable life safety system
- Flexible, on-demand isolation enables easy system expansion and modification
- Addressable isolation makes troubleshooting faster and easier
Siemens is the first and only UL fire product manufacturer to provide built-in isolation in all its major fire system devices at no extra cost. The ISOtechnology™ feature is built-in isolation technology that allows the system to continue to operate normally, even signaling the exact location of a short on the display and sounding an alarm in case of a detected emergency. Now standard on all Siemens fire safety devices and detectors, this feature provides real-time wire fault location reporting, reduced maintenance, and increased protection against short circuits for a more reliable life safety system.
Despite the critical importance of a fire safety system’s performance in protecting building occupants in the event of a fire or other building emergency, system designs often end up being based on the lowest possible installation and product cost. Wiring shorts or open circuits can render fire systems inoperable or significantly limit detection of fire events and therefore, potentially limit the ability to notify and evacuate building occupants.
“You shouldn’t have to pay a premium price for the best possible fire safety system performance. Protection matters – that is why we developed ISOtechnology – which includes short circuit isolation standard in every addressable device at no additional cost,” says Brian O’Mahoney, Segment Head for Fire Safety, Siemens Smart Infrastructure USA. “Part of what makes the ISOtechnology feature an industry game changer is that it allows engineers to provide Class X isolation, where each section of wire between every device is isolated and identifiable. This gives engineers design flexibility and significantly increases fire system performance, while dramatically reducing troubleshooting times by pinpointing signaling line circuit wiring problems – all of which reduces the overall project cost and improves life safety.”
Traditionally, many manufacturers require placing isolators between devices to “isolate” that section of wire. However, Siemens’ isolation technology that is built into its devices helps alleviate the need to install so many fire devices. This eliminates the need for extra labor, backboxes, and conduit, making the project overall more efficient. For instance, if 100 detectors were specified for a project, they would be installed plus 200 additional isolator modules, 200 backboxes and countless conduit – which more than doubles the materials’ cost and extends the project installation timeline. By contrast, only 100 detectors with the ISOtechnology feature would need to be installed to provide the same level of isolation.
Having fewer devices makes serviceability easier and more efficient. The standard loop configuration also increases functionality and survivability, with a short in one zone not affecting other zones or shutting down the entire system. Addressable isolation allows service providers to troubleshoot faster, pinpointing the exact location of a problem, avoiding disruptive testing, and decreasing business downtime.
In addition to not having to specify separate isolators, using less wiring and conduit also reduces material and related labor costs. And the flexible on-demand isolation allows end users to easily expand and modify their system whenever needed.
FOR MORE INFORMATION
To learn more about the ISOtechnology feature that is now standard on all Siemens fire safety devices and detectors, please visit https://sie.ag/3f98gZo.
ISOtechnology is a trademark of Siemens and/or its affiliates in some countries.
About Siemens
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. With around 71,000 employees worldwide, Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and its U.S. corporate headquarters in Buffalo Grove, Illinois, USA.
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global powerhouse focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. For more than 160 years, the company has innovated and invented technologies to support American industry spanning manufacturing, energy, healthcare and infrastructure. In fiscal 2019, Siemens USA reported revenue of $26.5 billion, including $1.23 billion in exports, and employs approximately 50,000 people throughout all 50 states and Puerto Rico.
Contacts for Journalists
Siemens
Allison Britt
Media Relations
+1-630-399-2587
Aynur Saltik
Media Relations
+1-312-560-3679