New Siemens RTU Solution Simplifies Efficiency for Small to Mid-size Buildings
Buffalo Grove, IL | March 4, 2021
- Improves energy efficiency, air quality, and building comfort
- Smart controller supersedes need for building automation solution
- Remote monitoring capability facilitates troubleshooting
- Allows for easy and fast commissioning
Siemens unveiled its Climatix® Rooftop Unit (RTU) optimization solution, designed for millions of smaller to medium-size buildings such as small offices, retail, grocery and convenience stores, restaurants, K-12 facilities, and houses of worship. This market relies mostly on basic thermostat control for heating and cooling and faces increasing pressures to reduce costs. The controller-driven solution addresses a gap in the market to improve energy efficiency, indoor air quality (including fresh air intake circulation), and overall building comfort – without having to add a complete building automation solution. It also includes remote management service that allows HVAC mechanical and controls contractors to gain real-time access to RTU performance data through the Internet, saving time and money by eliminating system downtime and unnecessary truck rolls.
“We set out to deliver a better rooftop unit management solution unlike any other that’s designed with efficiency in mind for both contractors and building owners,” stated John Karczmarczyk, Vice President, Siemens Smart Infrastructure USA. “This new solution has been tested and deployed working closely with our channel partners, to provide a true turnkey solution at an affordable price.”
RTUs have an average product lifespan of 15 to 25 years, with 90% of them continually running at a single fan speed regardless of need, creating inefficiencies. Without proper maintenance, equipment performance can decline over time, leading to poor indoor air quality, poor temperature management, nuisance noise, increased energy bills and unexpected system downtime with more costly repairs.
The Climatix RTU solution is designed for plug-and-play installation, with pre-terminated inputs and outputs reducing labor costs for contractors. The Climatix RT controller is pre-engineered with pre-defined applications designed specifically for RTUs and paired with Siemens sensors, the new Climatix VFD, and OpenAir® actuators to optimize installation, commissioning, and performance. The Climatix VFD has its sequence of operations specially programmed into the Climatix RT controller which helps contractors save hundreds of hours in training and commissioning.
During this pandemic time when indoor air quality and proper ventilation is critical, this new solution helps building owners address these concerns maximizing fresh outdoor air to the fullest extent possible, with three applications tailored to optimize indoor air quality and energy efficiency.
Climatix IC® remote management software works with the Climatix RT controller and the Climatix mobile app for RTU configuration, commissioning, and operations. The mobile app allows for secure monitoring, alarming, troubleshooting and program updates of equipment installed at multiple locations. Set points and schedules can also be adjusted remotely.
Remote connectivity makes commissioning new RTUs faster and easier -- even by junior technicians or apprentices working on their own. Remote monitoring also makes it easier to identify and troubleshoot potential system issues before dispatching service technicians onsite.
To learn more about the Climatix RTU solution, visit www.usa.siemens.com/rtu
Climatix, Climatix IC, and OpenAir are registered trademarks of Siemens and/or its affiliates in some countries.
About Siemens
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. With around 72,000 employees worldwide, Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and its U.S. corporate headquarters in Buffalo Grove, Illinois, USA.
Siemens Corporation is a U.S. subsidiary of Siemens AG, a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, Siemens Group USA generated revenue of $17 billion and employs approximately 40,000 people serving customers in all 50 states and Puerto Rico.
Siemens Contact for Journalists
Allison Britt
+1-630-399-2587