CNC4you Webinars
Don't miss our next event!
Setup and programming of a Turn-Mill B-axis lathe in G-code with programGuide
Friday, October 23, 2020
2:00pm Eastern / 1:00pm Central
Duration: 90-minutes
Mixed technology machine tools are becoming more popular every year in manufacturing. The process of combining milling and turning operations on the same machine not only improves part quality, but it also reduces manufacturing time.
The challenge, however, is programming such a complex machine. Once a B-axis rotary is added, it now becomes a 5-axis CNC machine. The SINUMERIK control, utilizing programGuide, has unique functionality designed specifically for this task.
In this webinar, we will have an opportunity to explore real-world programming examples that will take advantage of a 5-axis Turn-Mill.
First, we will utilize a common turning tool to jump between the main spindle and counter-spindle. A simple orientation of the B-axis and positioning of the milling spindle allow you to get the most out of your tooling. Next, we will explore milling operations on compound angles using the Cycle800 “swivel cycle” command. At the end of our session, you will have the confidence to apply this technology in your current manufacturing challenges.
Primary topics we’ll focus on during the webinar include:
- Setup of tools for a B-axis kinematic
- Moving the same turning tool from main spindle to sub-spindle operations
- Changing tool orientation to accommodate different part features
- Applying Cycle800 “swivel cycle” for drilling and milling operations
Archive
Case study between 3-axis and 5-axis machine technologies
Anywhere you look, you're going to find video content and advertisements of highly engineered multi-axis-capable machining centers. The synchronized motion of multiple axes working together can indeed be very mesmerizing.
But does this “WOW” factor carry over to the shopfloor? Does 'the more, the merrier' — in terms of machine axes — apply when the time comes to get the parts off the machine and out the door, or is this all just hype? Let's find out together.
Join us in this discussion where we'll analyze two sample machining processes, comparing the requirements and potential benefits of these two technologies.
Primary topics we’ll focus on during the webinar include:
- How to gain a better understanding of what each of these two machining technologies is capable of doing -- and doing well
- Key factors that can help you decide whether one technology will be more superior in your shop than the other
- How the SINUMERIK control’s multiple clamping functionality can help boost throughput by optimizing tool change strategies across multiple fixtures
_____________________________________________________________________________________________
Working with standard cycles in ShopMill using SINUMERIK 828D and 840D CNCs
When programming the SINUMERIK control utilizing the ShopMill conversational system, it's very helpful to take advantage of the vast selection of standard cycles.
Join us for this in-depth seminar where we'll take a detailed look at all these cycles — from deep hole drilling with a decremented peck depth to helical pocket milling.
At the conclusion of our online demonstration, you'll be able to start utilizing these cycles to their fullest potential.
Primary topics we’ll focus on during the webinar include:
- Drilling Cycles — centering, drilling, deep hole, boring and tapping
- Milling Cycles — facing, pocket, spigot, slot, thread milling and engraving
- Positions — random, pattern, bolt hole, obstacle, position repetition
- Creation of a sample program using many of these cycles
_____________________________________________________________________________________________
5-axis simultaneous machining with SINUMERIK 840D sl CNC
When moving into advanced technology, such as 5-axis machining, it's extremely important that you choose the best control for the application. The wrong choice can not only cost you time and money, but may even limit your overall capabilities.
This topic always leads to the final question — why choose the SINUMERIK CNC system from Siemens?
During this webinar, we'll dive into the world of 5-axis machining and attempt to answer this question. Through exploring both the advanced setup capabilities of the control as well as the key functions developed to optimize 5-axis toolpath, you'll begin to see what makes this CNC so special. So, join me in this unique opportunity to peek under the hood and see why you should choose Siemens.
Primary topics we’ll focus on during the webinar include:
- An overview of machining applications that require 5-axis toolpath
- Setup and operation of a 5-axis machine
- Unique commands that optimize CAM-based toolpath
- Key features in auto mode that allow operators to deal with such complex programs
_____________________________________________________________________________________________
Advanced milling cycles for ShopMill and programGuide using SINUMERIK 828D and 840D controllers
Long gone are the days of having to rely on an expensive CAM software package or being able to recite the entirety of available G-codes from front to back in order to create the correct toolpaths to machine your part.
While conversational programming is nothing new, the integrated milling cycles of the SINUMERIK 840D sl and 828D utilize advanced functions, such as gouge detection, residual material, and irregular stock machining (just to name a few) — and these functions will take your shop-floor programming to the next level.
Join us for this webinar and get a glimpse of which advanced milling cycles are available to you, and also to see some real-life application examples which you can implement on your shop-floor today.
Primary topics we’ll focus on during the webinar include:
- How to create a part program using the path milling, spigot and pocket cycles
- Programming in ShopMill as well as programGuide
- Using the residual material cycle to handle machining areas not previously reached
- How to verify part programs through built-in simulation
_____________________________________________________________________________________________
Creating a post-processor for SINUMERIK 840D sl and SINUMERIK 828D (milling)
One of the most critical puzzle pieces when looking at the manufacturing process chain is the post-processor. It's also one of the most overlooked and under-estimated. Even with a precision CNC machine and an advanced CAD/CAM system, your products will only be as good as the post-processor translating it.
Join us and dive into the world of post-processing. Let’s discuss all the critical commands as well as program formatting that will allow your SINUMERIK control to achieve its highest potential. No matter what CAM system you're using, this webinar will give you the tools and knowledge to know exactly what you need your post-processor to output.
Primary topics we'll focus on during the webinar include:
- Program structure and format
- Key G- and M-codes and how to apply them
- What cycles need to be supported and why
- Common mistakes when developing posts for the SINUMERIK CNC
_____________________________________________________________________________________________
Setup and programming of a fourth-axis machine in G-code with programGuide —
(SINUMERIK 840D sl / 828D)
When making the move into more advanced technology, most companies look to transition to a fourth axis mill as a first step. This type of kinematic setup can allow users to begin to work on multiple sides of a part as well as multiple fixtures. The SINUMERIK control is equipped with several different embedded functions that allow for quick, simple setup and programming on the shop floor or through a CAM system.
During this webinar, we will have an opportunity to explore real-world programming examples that will take advantage of both milling and drilling on a fourth axis — from drilling holes around the peripheral of a part to wrapping milling features about a diameter. We’ll look at both vertical and horizontal milling setups. At the conclusion, you’ll have the confidence to apply this technology to your current challenges.
Primary topics we'll focus on during the webinar include:
- Setup of a 4-axis mill — vertical and horizontal kinematic
- Shopfloor G-code programming through programGuide
- External programming through a CAM system
- Milling on multiple sides of a part
- Peripheral drilling on-center and off-center
- Milling with cylinder surface transformation
- Tool setup with either positive or negative offsets
_____________________________________________________________________________________________
Utilizing the new Mastercam-certified Siemens post for 4-axis milling —
SINUMERIK 840D sl and 828D
When working with external programming systems, one of the most important pieces to ensuring success is the post processor. In an effort to achieve the best possible performance of both the CAD/CAM system and the CNC, Mastercam and Siemens have continued to work together to develop a new 4-axis milling post.
In this session, we'll see the unique features that have been integrated, as well as how to modify the post to make it fit your needs. During this session, we will look at both 3+1 plane milling operations and multi-axis tool paths.
Primary topics:
- CYCLE 832 support for high-speed settings — now with the latest Top Surface functionality
- Drill cycles (CYCLES 82, 83, 84, 85, 86, 840) — with full 4-axis support
- WORKPIECE output for graphical simulation — including rotary axis blank orientations
- Siemens 4-axis application guide
- Optimized multi-axis tool path utilizing the FGROUP and FGREF commands
- Streamlined program editing with the GROUPS functionality
_____________________________________________________________________________________________
Part probing in auto-mode with ShopMill — SINUMERIK 840D sl and 828D (milling)
When setting up a milling machine, speed and accuracy can directly lead to profitability. This is a key reason why integrated probes have become almost mandatory in today’s top shops. The next logical step is to leverage this technology to ensure quality throughout your production run. In-process probing during running in auto-mode is a great way to adjust for setup inaccuracies as well as quality controlling parts during production.
In this webinar, we'll have an opportunity to explore real-world programming examples that will utilize the part probing functionality native to the SINUMERIK control. First, we'll look at how to calibrate and utilize probes in your setup process. Next, we'll explore creating conversational ShopMill programs that will apply the SINUMERIK built-in probing routines while running in auto mode. Once complete, you'll have the confidence to apply this technology in their current challenges.
Primary topics:
- Initial part probe setup and calibration
- Utilizing the probing cycles in Jog for measuring and work coordinate setting
- Programming and running of the standard measuring cycles through ShopMill
- Capturing of measuring data for reporting
_____________________________________________________________________________________________
Shopfloor programming with ShopMill (SINUMERIK 840D sl and 828D — milling)
Whether you’re planning to handle all of your part programming at the machine tool’s control or just some of the more basic tasks, utilizing the CNC system’s intuitive conversational programming will make you much more proficient.
ShopMill has been designed to allow quick programming of even complex tool paths through a variety of integrated cycles. From 2-axis basic milling to 5-axis multi-sided programming, this interface gives you the edge that you need.
In this webinar, we'll have an opportunity to explore real-world programming examples that utilize the ShopMill programming interface. First, we’ll look at how to program a basic part with the standard milling and drilling cycles. Second, we’ll explore creating more complex tools paths with our contour milling cycles.
Once complete, attendees will have the confidence to apply this technology in their current challenges.
Primary topics:
- Hole-making with standard drilling cycles
- Pocket and profile milling with standard milling cycles
- Part engraving and serial numbering
- Advanced irregular contour milling and pocketing
_____________________________________________________________________________________________
Part programming in auto-mode with programGuide (SINUMERIK 840D sl and 828D)
Setting up a milling machine utilizing a digital part probe has become commonplace in today’s job shops. However, not many shops are taking advantage of these tools while the machine is producing parts. In-process probing while running in auto mode is a great way to adjust for setup inaccuracies as well as quality controlling parts during production.
During this webinar, we’ll have an opportunity to explore real-world programming examples that will utilize the part probing functionality native to the SINUMERIK control. First, we’ll look at how to program and run the built-in probing cycles. Next, we’ll explore the creation of some custom measuring routines. Once complete, you will have the confidence to apply this technology in your current machining challenges.
Primary topics:
- Initial part probe setup and calibration
- Utilizing probing cycles for measuring and work coordinate setting
- Programming and running of standard measuring cycles
- Creation of custom measuring routines utilizing the MEAS command
- Capturing of measuring data for reporting
_____________________________________________________________________________________________
New DXF programming in version 4.7 for SINUMERIK 840D sl and 828D
It's very common in today’s manufacturing environment to be working directly from electronic DXF prints. In many cases, the details required to explain part geometry may be too complex to create a traditional CAD print. Also, human error can be avoided when programming by removing the data entry portion of a program. In this webinar, we will demonstrate the new, fully-integrated DXF option for software version 4.7.
Users will now be able to bring DXF files directly into the SINUMERIK control without the need for external software. We’ll create a ShopMill program (conversational), as well as a programGuide part program (G-code) utilizing a DXF file. Once complete, attendees will have a good understanding of the steps required to program the SINUMERIK control directly from a DXF file.
Primary topics:
- Setup of the DXF-Reader for ShopMill and programGuide part programming
- Establishing a part zero in the DXF-Reader
- Selecting both profiles and hole locations for adding to a main program file
- Viewing and modifying the output data
- Editing, simulating and running of programs
_____________________________________________________________________________________________
5-axis (3+2) G-code programming with programGUIDE in SINUMERIK Operate (840D sl and 828D)
This webinar is designed to show a user how to leverage 5-axis machining technologies in the demanding markets of the job shop. The course is intended to give users the ability to both create G-code programs at the control, as well as understand critical cycles that will be used by your post-processor when creating CAD/CAM-based programs.
We will first look at the key functions within the Siemens control that aid in dramatically simplifying the tasks of setting up a 5-axis machine. Through leveraging such cycles like Align Edge and Align Plane, we can demonstrate how these functions will reduce setup time and increase productivity. Once the part has been setup, we will explore how to handle 5-axis part programming in G-code directly on the control. Attendees will be able to see a basic part program created, simulated and run in auto mode, giving an excellent understanding of the entire process from setup through part production.
Primary topics:
- Setup of 5-axis parts in jog mode
- Key features at the work coordinate level that simplify working with 5-axis parts
- 5-axis part program creation through programGUIDE
- Simulation of the created part for verification purposes
- Review of the same part methodized in a CAD/CAM system
- Running the created part program in Auto while demonstrating key features
_____________________________________________________________________________________________
Automatic calculations when missing information for ShopMill (840D sl and 828D)
How often do you find when programming a part that not all of the necessary dimensional information is included? This can create disruption to the programming process and cost both time and money. The SINUMERIK control has the ability to figure out this missing information for you and automatically apply it, where needed.
This webinar will guide attendees through creating a program from a print that has critical information missing. Once completed, you will be able to start utilizing this advanced functionality.
Primary topics:
- Auto calculations in the contour editor
- Defining tangency between elements
- Mathematic calculations in numerical fields
- Utilizing the built-in calculator
_____________________________________________________________________________________________
Utilizing your 4-axis mill to its fullest with ShopMill
When making the move into more advanced technology, most companies look to transition to a 4th-axis mill as a first step. This type of kinematic setup can allow users to begin to work on multiple sides of a part as well as multiple fixtures. The SINUMERIK control is equipped with a number of different embedded functions that allow for quick, simple setup and programming on the shopfloor.
In this webinar, we will have an opportunity to explore real-world programming examples that will take advantage of both milling and drilling on a 4th axis. From drilling holes around the peripheral of a part to wrapping milling features about a diameter. We will look at both vertical and horizontal milling setups. Once complete, attendees will have the confidence to apply this technology in their current challenges.
Primary topics:
- Setup of a 4-axis mill – vertical and horizontal Kinematic
- Milling on multiple sides of a part
- Peripheral Drilling on center and off-center
- Milling with cylinder surface transformation
- Setting up tools with either positive or negative offsets
_____________________________________________________________________________________________
Variable programming with ShopMill and programGuide for the SINUMERIK 840D sl and 828D
It's a natural progression when beginning to master standard programming of a CNC to start exploring more advanced techniques. Inevitably, this will lead you to variable-based programming, an advanced method of programming that utilizes instructional statements with definable variables to quickly change the result of a program.
Join us in exploring various methods and techniques to create such programs. We will look at utilizing both pre-defined variables, as well as creating our own unique ones. Next, we'll apply these variables to real-world examples, like adapting a conversational-based program to handling a family of parts and creating custom G-code routines.
Primary Topics
- Utilizing standard “R” variables
- Creation of local and global custom variables
- Methodizing a ShopMill part program to utilize variables
- Create a custom G-code routine to check for tool breakage
_____________________________________________________________________________________________
Working with standard cycles in programGuide (G-code) for milling in SINUMERIK 840D sl and 828D
When programming the SINUMERIK CNC in G-code, it’s very helpful to take advantage of the vast selection of standard cycles. This is even more true when using a CAM system and trying to take advantage of the full power of the control. During this seminar, we will take an in-depth look at all of these cycles — from deep hole drilling with a decremented peck depth to helical pocket milling. Once complete, attendees will be able to start utilizing these cycles to their fullest potential.
Primary Topics
- Drilling cycles — centering, drilling, deep hole, boring, tapping
- Milling cycles — facing, pocket, spigot, slot, thread milling, engraving
- Positions — random, pattern, bolt hole, obstacle, position repetition
- Creation of a sample program using the above cycles
_____________________________________________________________________________________________
Working with Standard Cycles in ShopMill with SINUMERIK Operate for SINUMERIK 840D sl and 828D
When programming the SINUMERIK control utilizing the ShopMill conversational system it is very helpful to take advantage of the vast selection of standard cycles. During this seminar we will take an in-depth look at all of these cycles. From deep hole drilling with a decremented peck depth to helical pocket milling. Once complete, attendees will be able to start utilizing these cycles to their fullest potential.
Primary Topics
- Drilling Cycles — centering, drilling, deep hole, boring, tapping
- Milling Cycles — facing, pocket, spigot, slot, thread milling, engraving
- Positions — random, pattern, bolt hole, obstacle, position repetition
- Creation of a sample program using the above cycles
_____________________________________________________________________________________________
DXF programming in ShopMill and programGuide for SINUMERIK 840D sl and 828D
It’s very common in today’s manufacturing environment to be working directly from electronic DXF prints. In many cases,
the details required to explain part geometry many be too complex to create a traditional CAD print. Human error can also be avoided when programming by removing the data entry portion of a program.
During this webinar, we will be demonstrating the process of programming the SINUMERIK CNC from a DXF file. We will create a ShopMill (conversational) program as well as a programGuide (G-code) part program. Once complete, attendees will have a good understanding of the steps required to program a SINUMERIK control directly from a DXF file.
What you will learn:
- Setup of the HMI CAD-Reader for ShopMill and programGuide part programming
- Establishing a part zero in the CAD-Reader
- Selecting both profiles and hole locations for adding to a main program file
- Opening data in the machine control and adding necessary elements to create the program
- Editing, simulating and running of programs
_____________________________________________________________________________________________
Working with CAD/CAM-based programs and applying the high-speed CYCLE832 function in SINUMERIK 840D sl and 828D CNC
This webinar is intended to show a machine tool user how to begin leveraging CAM-based programs on Siemens CNC-equipped machines. We will take an example of a part that has been posted out in both the Siemens and ISO (Fanuc) protocols and cover the entire process from importation of the file through execution in Auto-mode. Next, we will look at utilizing sub-program structured code to better optimize working with complex part programs. Finally, we will leverage the high-speed Cycle832 function to improve the performance of the program. Once completed, attendees will have a good understanding of what it takes to program and run a SINUMERIK 840D sl and 828D-controlled milling machine from programs created outside of the control.
What you will learn:
- How to import CAD/CAM programs into the control
- Switching between Siemens and ISO (Fanuc-style) modes
- Using sub-program techniques to better manage your part programs
- Working with files located externally to NC memory
- How to edit, simulate and run programs
- Applying the CYCLE832 high-speed function to a part program and running in Auto-mode
____________________________________________________________________________________________
5-axis machining in the job shop with SINUMERIK Operate for 840D sl and 828D
Programming with Cycle800 is designed to show a machine tool user how to leverage 5-axis machining technologies in the demanding markets of the job shop. We will first look at the key functions within the Siemens control that aid in dramatically simplifying the tasks of setting up a 5-axis machine. Then, through leveraging such cycles like Align Edge and Align Plane, we can demonstrate how these functions will reduce setup time and increase productivity. Once the part has been setup, we will explore how to handle 5-axis (3+2) part programming directly on the control. At the conclusion of the webinar, you will be able to see a basic part program created, simulated and run in auto mode.
What you will learn:
- Setup of 5-axis parts in jog mode
- Key features at the work coordinate level that simplify working with 5-axis parts
- 5-axis part program creation through ShopMill
- Simulation of the created part for verification purposes
- Review of the same part methodized in G-code with ProgramGuide
- Running the created part program in auto while demonstrating key features
_____________________________________________________________________________________________
G-code programming with programGuide for milling in SINUMERIK Operate for 840D sl and 828D
Programming the SINUMERIK 840D sl and 828D controls with programGuide for milling is intended to step a user through the basics of G-code programming using SINUMERIK Operate. Attendees will get an opportunity to see a basic 2-D milled part programmed, simulated and run. We will create new tools in the offset table, as well as review the steps required to set the offset of such tools. In the second part of the webinar, we will review a more complex part program that shows examples of profile milling, irregular pocketing and upper-level commands. Upon completion of the seminar, a user should have a good understanding of programGuide and how to create G-code programs in the SINUMERIK Operate graphical user interface.
What you will learn:
- Creation and setup of milling tools
- G-code programming of a 2-D part
- Verifying the completed program through simulation
- Using upper-level commands like sub-routines, feed per rev/feed per tooth and TOFFL / R for modifying offsets
- Running programs in auto and utilizing functions like Repos mode, and Block Search mode
_____________________________________________________________________________________________
Working with CAD/CAM-based programs and applying the high-speed CYCLE832 function for SINUMERIK 808D milling
Working with CAD/CAM-based part programs and applying the high-speed cycle for SINUMERIK Operate 808D milling is intended to show a CNC user how to begin leveraging CAM-based programs on SINUMERIK 808D-equipped machines. We will take an example of a part that has been posted out in both the Siemens and ISO protocols while covering the entire process from importation of the file through execution in Auto mode. Next, we will leverage the high-speed CYCLE832 function to improve program performance. Once completed, attendees will have a good understanding of what it takes to program and run a SINUMERIK 808D milling machine from programs created outside of the control.
What you will learn:
- Importing of CAD/CAM programs into the control
- Switching between Siemens and ISO modes
- Editing, simulation, and running of part programs
- Applying the CYCLE832 high-speed function to a part program and running in Auto mode
_____________________________________________________________________________________________
Commonality of programming for SINUMERIK Operate for SINUMERIK 840D sl and 828D
Commonality of Programming for SINUMERIK Operate (milling) is intended to show a user how similar functionality is between the creation of programs in either ShopMill, G-code with programGuide mode, importing from a CAD / CAM system, or running programs previously created for an ISO-style control. We will take one example of a part and show it programmed in all four ways and then run each of them in Auto mode. Once completed, attendees will have a good understanding of what it takes to program and run a Siemens SINUMERIK-controlled milling machine from programs created inside and outside of the CNC.
What you will learn:
- Programming and simulation in ShopMill
- Programming and simulation in G-code with programGuide
- Importing, editing and simulation of programs created in a CAD / CAM system
- Importing, editing and simulation of programs in an ISO-compatible CNC
_____________________________________________________________________________________________
An overview of Easy CNC with ShopMill — setup and programming with SINUMERIK Operate for SINUMERIK 840D sl and 828D
Easy CNC ShopMill is intended to step a novice user through the process of setting up a basic 3-axis milling machine. Once setup is complete, we will then create a part program through our ShopMill programming option and verify its functionality within the built-in simulation. Final steps will then emulate the machine running in a virtual automatic mode. At the end, you will have a good understanding of what it takes to program and run a Siemens CNC-controlled 3-axis mill.
What you will learn:
- Manual moving of the machine tool in Jog mode
- Setting up of a part zero and tool offsets in Jog mode
- Programming of a job in ShopMill
- Verifying the created part program through simulation
_____________________________________________________________________________________________
Setup and programming with the SINUMERIK 808D Milling control
Easy CNC is intended to step a novice user through the process of setting up a basic 3-axis milling machine. Once setup is complete, we will then create a part program through our programGUIDE programming interface and verify its functionality within the built-in simulation. The final steps will then emulate the machine running in a virtual automatic mode. Once completed, you will have a good understanding of what it takes to program and run a SINUMERIK 808D 3-axis mill.
What you will learn:
- Setting up a part zero and tool offsets
- Programming of a job in programGUIDE
- Verifying the created part program through simulation
- Running the created job in auto-mode
_____________________________________________________________________________________________
Advanced milling cycles for the SINUMERIK 828D and 840D sl CNCs
Advanced Milling Cycles for SINUMERIK Operate will go through the process of programming a part utilizing the systems contour profile cycle, pocket cycle, and spigot cycle. This example will be first programmed with the ShopMill conversational interface and then programmed in G-code utilizing our programGUIDE interface. Once completed, attendees will have a good understanding of what it takes to program advanced cycles in both ShopMill and programGUIDE.
What you will learn
- Creating a part program using the path milling, spigot, and pocket cycles
- The example will be programmed in both ShopMill and programGUIDE
- Use the residual material cycle to handle machining areas not previously reached
- Verifying the created part programs through built-in simulation
_____________________________________________________________________________________________
Programming a lathe with C-axis and Y-axis in G-code programGuide —
SINUMERIK 840D sl / 828D (turning)
As mixed technology becomes more mainstream in today’s manufacturing, it’s critical to understand all of the capabilities your SINUMERIK control has to offer. When looking in from the outside, these complex turning centers can appear intimidating. SINUMERIK CNC, however, has incorporated several high-level commands that simplify the complexity of these G-code part programs.
In this webinar, we’ll have an opportunity to explore a real-world programming example that will take advantage of both C-axis and Y-axis functionality utilizing the TRANSMIT and TRACYL commands — from face drilling offset holes to peripheral milling of unique features. By the end of the session, you’ll have the confidence to apply this technology in your current manufacturing challenges.
Primary topics:
- Face drilling operations with either C- or Y-axis
- Peripheral drilling on-center and off-center
- Applying the milling cycles for face and peripheral machining
- Key challenges when setting up tools and offsets
_____________________________________________________________________________________________
Multi-channel machining with ShopTurn — SINUMERIK 840D sl and 828D (turning)
What does multi-channel machining mean to you? Perhaps it’s the next step for staying competitive? Together we’ll explore this unique technology and learn how this advanced capability can allow shops to proceed to the next level.
During this webinar, you’ll have the opportunity to explore the operation and programming of a multi-channel machine tool first-hand. By utilizing the ShopTurn conversational programming environment, we’ll program complex tasks with ease. From managing multiple programs that will run simultaneously with the job list tool, to adding wait functions that control the timing of the channels. Once complete, you’ll have a much better understanding of what this technology is about and if it truly is the next step in shopfloor manufacturing.
Primary topics:
- Setup and construction of multi-channel machine tools
- Benefits and challenges of multi-channel machining
- Creation of a job list for managing the part programs in the channels
- Programming wait commands to align the timing between channels
- Controlling the operations through the group functionality
_____________________________________________________________________________________________
Setup and program turn-mill B-axis lathes in ShopTurn — SINUMERIK 840D sl and 828D (turning)
Mixed technology machine tools are becoming more popular every year in manufacturing. The process of combining milling and turning operations on the same machine not only improves part quality, but also reduces manufacturing time. The challenge; however, is programming such a complex machine. Once a B-axis rotary is added, it becomes a 5-axis machine tool. The SINUMERIK control, utilizing ShopTurn, has unique functionality designed specifically for this task.
In this webinar, we’ll have an opportunity to explore actual programming examples that will take advantage of a 5-axis turn-mill machine. First, we’ll utilize a common turning tool to jump between the main spindle and counter-spindle. A simple orientation of the B-axis and positioning of the milling spindle allow you to get the most out of your tooling. Next, we’ll explore milling operations on compound angles using the Cycle800 “swivel cycle” command. Once complete, attendees will have the confidence to apply this technology in their current challenges.
What you will learn:
- Tool setup for a B-axis kinematic
- Moving the same turning tool from main spindle to sub-spindle operations
- Changing the tool orientation to accommodate different part features
- Applying the Cycle800 “swivel cycle” for drilling and milling operations
_____________________________________________________________________________________________
Setup and programming sub-spindle lathes in ShopTurn — SINUMERIK 840D sl and 828D (turning)
As machine tools become more advanced in their functionality, it's critical to understand all of the capabilities your SINUMERIK CNC has to offer. When looking in from the outside, these complex turning centers can appear intimidating; however, once you see how simple it is to utilize these advanced capabilities in ShopTurn, you'll be applying them on a daily basis.
In this webinar, we'll have an opportunity to explore real-world programming examples that will take advantage of a machine equipped with a sub-spindle. First, we'll look at how to setup a sub-spindle lathe and then we'll program a part. Simple part transfers to include part-off and drawing capabilities. Once complete, attendees will have the confidence to apply this technology in their current manufacturing challenges.
Primary topics:
- Setup of tools and work offsets for both main- and sub-spindle applications
- Turning a complete part with a transfer to the sub-spindle
- Handling bar work by including a part-off cycle with a part transfer
- Drawing the part out of the main spindle prior to part-off
_____________________________________________________________________________________________
Programming a lathe with C-axis and Y-axis in ShopTurn — SINUMERIK 828D and 840D sl (turning)
As mixed technology becomes more mainstream in today’s manufacturing, it is critical to understand all of the capabilities your SINUMERIK CNC has to offer. When looking in from the outside, these complex turning centers can appear intimidating. However, once you see how simple it is in ShopTurn to utilize these advanced capabilities, you will be applying them on a daily basis.
In this webinar, we will have an opportunity to explore real-world programming examples that will take advantage of both C-axis and Y-axis functionality — from face-drilling offset holes to peripheral milling of unique features. Once complete, attendees will have the confidence to apply this technology in their current machining challenges.
Primary Topics:
- Face-drilling operations with either C- or Y-axis
- Peripheral drilling on-center and off-center
- Applying the milling cycles for face- and peripheral machining
- Key challenges when setting-up tools and offsets
_____________________________________________________________________________________________
ID Part Programming in ShopTurn for SINUMERIK 840D sl and SINUMERIK 828D
At an initial glance, one would think that ID part programming is the same process as OD programming. However, with further inspection you will see that special precautions must be taken into account. For instance, is there a hole already in the part to start machining from. If so how can I control my boring bar from clipping the backside of this hole while performing the ID machining operation? In this webinar, you will explore multiple scenarios and the steps taken to ensure a successful part program. Once completed attendees will have an intimate understanding of how to handle part programs with ID features.
Primary Topics:
- Centric Drilling Cycles – Centering, Drilling, Deep hole
- ID Turning using standard cycles
- ID Turning using the contour turning cycles
- Key machine parameters for controlling the resulting tool path
_____________________________________________________________________________________________
Working with advanced cycles in ShopTurn for SINUMERIK 840D sl and SINUMERIK 828D
This webinar is intended to show a machine tool user how to begin applying strategies that will make their part programs even more efficient. This is ShopTurn-based programming utilizing advanced functions like gouge detection, residual material, and irregular stock machining to name a few. Next, we will begin to explore feed optimization, as well as different cutting strategies. This course will take your ShopTurn programming to the next level.
What you will learn:
- Tool creation with full geometry description
- Contour turning with pockets for insert checking and gouge detection
- Applying the residual material detection cycle
- Advanced feed strategies for chip handling and reducing insert notching
- Working with cast or pre-machines blanks
- Contour grooving and plunge turning applications
_____________________________________________________________________________________________
Basic setup and programming of SINUMERIK 808D in turning applications
This webinar is designed to teach you basic setup and programming principles of the SINUMERIK 808D in turning applications. First, we'll begin with the creation and setup of tools. Next, we'll methodize a part program through the programGuide user interface. Then we'll demonstrate the use of standard cycles and create a turning routine for an irregular shape. Lastly, we'll verify the program through onboard simulation and run it in auto mode. Upon completion of this webinar, a user will have a good understanding of the necessary steps to program and operate the SINUMERIK 808D in turning applications.
What you will learn:
- Creation of tools and offsets
- Creation and part program management through the program manager function
- Editing, simulation and running of programs
- Using standard and advanced cycles applied to a specific part
_____________________________________________________________________________________________
G-code programming with programGuide for turning in SINUMERIK Operate for 840D sl and 828D
Programming with programGuide for turning is intended to step a user through the basics of G-code programming in the Siemens SINUMERIK Operate graphical user interface. Attendees will get an opportunity to see a basic 2-D turned part programmed, simulated and run. We will create new tools in the offset table, as well as review the steps required to set the offset of such tools. In the second part of the webinar, we will review a more complex part program that shows examples of C-axis drilling and milling utilizing upper-level commands. Upon completion of the seminar, a user should have a good understanding of programGuide and how to create G-code programs in the SINUMERIK Operate graphical user interface.
What you will learn:
- Creation and setup of turning and milling tools
- G-code programming of a 2-D lathe part
- Verifying the completed program through simulation
- Using upper level commands like TRANS and TRACYL for C-axis work
- Running programs in auto and utilizing functions like Repos mode, and Block Search mode
_____________________________________________________________________________________________
Easy CNC with ShopTurn — setup and programming with SINUMERIK Operate for SINUMERIK 840D sl and 828D
This webinar is intended to step a novice user through the process of setting up a basic, 2-axis turning machine. Once setup is complete, we will then create a part program through the ShopTurn programming option and verify its functionality within the built-in simulation. During the final step, we will emulate the machine running in a virtual automatic mode. After this webinar session, you will have a good understanding of what it takes to program and run a SINUMERIK-controlled 2-axis turning machine.
What you will learn:
- Setup of a job through the intuitive standard function of Jog mode
- How to create and manage tools and offsets in the Offset tables
- Programming of a job through the ShopTurn user interface
- Verifying the created part programs through built-in simulation
- Running the part program and exploring key advanced functions in Auto modeText
_____________________________________________________________________________________________
Setup and programming sub-spindle lathes in G-code with programGuide SINUMERIK 840D sl and 828D
As machine tools become more advanced in their functionality, it’s critical to understand all of the capabilities your SINUMERIK CNC has to offer. When looking in from the outside, these complex turning centers can appear intimidating. However, once you have a basic understanding of the G-codes driving this technology, it becomes much easier to support these machines through a CAM solution.
In this webinar, we’ll have an opportunity to explore real-world programming examples that will take advantage of a machine tool equipped with a sub-spindle. First, we will look at how to set up a sub-spindle lathe and then program apart. Simple part transfers to including part-off and drawing capabilities. Once complete, attendees will have the confidence to apply this technology in their current challenges.
Primary topics we'll focus on during the webinar include:
- Setup of tools and work offsets for both main and sub-spindle applications
- Turning a complete part with a transfer to sub-spindle.
- Handling bar work by including a part-off cycle with a part transfer
- Drawing the part out of the main spindle prior to part-off
_____________________________________________________________________________________________
SINUMERIK Service and Maintenance 101 — Tips and tricks to maintaining and troubleshooting your Siemens CNC
Have you ever wondered what those extra screens on your SINUMERIK operator panel are for? We spend so much time operating our machines that it becomes too easy to overlook the onboard tools available in the control. In fact, if you wait until an issue arises, then you’re probably too late.
Join us for this in-depth session and we’ll show you how to troubleshoot and maintain your SINUMERIK control. Machine tool CNCs are complex pieces of equipment, but when you use the tools available at your fingertips, even the most novice user can achieve success. The more you learn about the SINUMERIK CNC, the more you’ll love it!
Primary topics we’ll focus on during the webinar include:
- System hardware overview
- Backups and recoveries
- License and option management
- Navigation for troubleshooting and maintenance
- Onboard tools and diagnostics
_____________________________________________________________________________________________
Where to go when you need help with your SINUMERIK CNC
Navigating the world of Siemens can be quite a daunting task. With such a large product portfolio, we tend to reach into many areas of the global market space. In turn, there is a flood of information, so how can you find what is most important to you?
Our next webinar will explore how to navigate the waters of Siemens to find the best support for the SINUMERIK control. We’ll review four main areas from the perspective of end-users, machine tool dealers and even machine tool builders. At the completion of the session, you’ll have a much better understanding of the many resources available to help you support the Siemens control.
Primary topics we'll focus on during the webinar include:
- Service and Support — web-based tools, hotline, local resources
- Operation and Programming — websites, online and in-person training
- Available Tools — Access MyMachine, Create MyConfig, SINUTRAIN
- Available Programs — warranty terms, extended warranty, service contracts, machine registration
_____________________________________________________________________________________________
Preventative maintenance for SINUMERIK 840D sl and 828D CNC
The control preventative maintenance webinar for the SINUMERIK 840D sl and 828D CNCs is designed to step a user through key procedures that aid in the backup and recovery of a system. From backups and restorations of controls, part programs and tool offset tables, to reviewing alarm messages and the navigation of supporting documentation to diagnose an issue. We will also review the proper procedure for control registration to ensure that the full warranty can be achieved, as well as showing the benefits of our internal logbook and automatic BOM generation. Upon completion, SINUMERIK CNC users will have a good understanding of the steps required to maintain a healthy recoverable system.
What you will learn:
- Control Archive generation and restoration
- Part programs and offset table backups
- Alarm diagnosis
- Machine registration
- Log book utilization and BOM generation
- Machine data navigation and application
_____________________________________________________________________________________________
Learn the fundamentals of ISO compatibility mode (G291) — SINUMERIK Operate for 840D sl, 828D and 808D controls
When a machine shop adds a new CNC to its manufacturing floor, employees will often need to change their entire programming process. This leads to a longer learning curve as well as incompatibilities of existing part programs.
What would you say if we told you that the SINUMERIK CNC has the capability of running ISO-based programs with little or no modification?
Well, that G81 code that you know, and love can still be used. In fact, most ISO-based cycles for milling and turning applications will run simply by activating G291.
Join us for an interactive demonstration where we’ll show you how to use the ISO-compatible mode on a turning machine. Not only will you learn how to setup and run these ISO-based programs, we’ll also explore how you can take this programming to the next level.
Primary topics we’ll focus on during the webinar include:
- Fundamentals of ISO compatibility (G291)
- ISO version A, B, C compatibility
- Mixing programming languages
- Sub-routine calls ISO
_____________________________________________________________________________________________
Program and operate your SINUMERIK 828D and 840D CNC machines with ease
You already know that the SINUMERIK CNC is a highly innovative control platform that offers proven superiority in many advanced machining applications. But did you ever think that such a sophisticated control could be really easy-to-use?
Well, SINUMERIK's graphical user interface offers you new, powerful functions — for example, machining step and high-level language programming can be combined in one user interface. When you setup a workpiece, measurements are clearly displayed using on-screen animations. Different kinematics can be easily setup. And complex workpieces can be machined in just one clamping operation. Simply put — programming and operation has never been easier.
Discover the many tips, tricks and shortcuts of the SINUMERIK 828D and 840D sl CNCs and harness the full potential of your Siemens control.
Primary topics we'll focus on during the webinar include:
- Functions – soft keys – short keys
- Position commands
- Sub-programs and loops
- Feed, spindle and transformation commands
- Auto-mode
- And more...
_____________________________________________________________________________________________
Real-time machine optimization for your CNC
Adaptive Control Monitoring (ACM) monitors and optimizes performance by measuring cutting torque in real-time and automatically adjusting feed-rates to maximize efficiency. Each machining operation is optimized in real-time and can account for variations in raw material, changing machining conditions, dimensional variation and much more.
During this webinar, we'll discuss the next steps in machine optimization with ACM. We'll explore its functionality, sight real-world cases where reductions of over 40% in cycle times have been seen, and explore tool life extensions of over 300%. See what's possible when you begin to leverage the power of Siemens.
Primary topics we'll discuss include:
- Capability of Adaptive Control and Monitoring
- Practical application
- Cycle time reduction and tool life extension
- Collision detection and mitigation
- Common mistakes when developing posts for SINUMERIK
_____________________________________________________________________________________________
Advanced variable programming with programGuide — SINUMERIK 840D sl / 828D
It’s a natural progression when beginning to master standard programming of a CNC and to start exploring more advanced techniques. Inevitably, this will lead you to variable-based programming, an advanced method of programming that utilizes instructional statements with definable variables to quickly change the outcome of a program.
As a result of the popularity of our first variable programming webinar, we’ve created this next seminar as a continuation of the topic. We will explore deeper into the structure and the use of logic statements, the creation, and re-mapping of custom M- and G-codes, as well as custom alarms and messages.
Next, we’ll apply these new skills to the creation of a custom cycle, which will allow machine users to push variables from a main program to a sub-program. By the end of our session, you‘ll gain a much more in-depth understanding of variable programming.
Primary topics we'll focus on during the webinar include:
- Structure and use of logic statements
- Custom user alarms and messages
- Creation and reassignment of M- and G-code commands
- Creation of custom cycles
_____________________________________________________________________________________________
Enabling and protecting your digital manufacturing
As companies move into the age of digitalization, are they becoming more vulnerable? How can we protect our information all the way down to the CNC level? Join us in exploring how our partner, Identify3D, is answering these tough questions and more.
With the increased digitalization of manufacturing processes, the protection and control of manufacturing data is becoming quite significant. Whether for internal or contracted production, manufacturing IP (designs, G-code, bill of process, etc.) is in danger of getting into the wrong hands and even being misused.
In our next webinar, we'll introduce the work we’ve been doing with Identify3D to bring security, repeatability, and traceability into your digital manufacturing process. We'll show an end-to-end demonstration, from design to CNC manufacturing, and then we'll highlight how to protect sensible data, associate business and manufacturing policies, enforce those policies, and leverage the complete digital history of such process.
Primary topics we'll focus on during the webinar include:
- Manufacturing data protection
- Manufacturing data usage control — all through the supply chain
- Enforcing rules at the machine level through the SINUMERIK control
- Digital history visibility
_____________________________________________________________________________________________
Digitalization — you're closer than you may think
It seems like almost every day we hear something about Digitalization, Industry 4.0, the Internet of Things or some variation thereof. But what does this actually mean, and more importantly, how can you ensure that you’re not left behind?
Digitalization can be a very overwhelming discussion; however, you may be a lot closer to it than you think.
Join Ramona Schindler, Digitalization Business Development Manager, in exploring how Digitalization is not only for the large enterprise but in fact is already occurring in small manufacturing businesses today.
See how simple steps can begin to move you further down this road leading to more efficient and profitable production.
.
Primary topics of the webinar include:
- Finding out how you can position yourself on the road to Digitalization
- Discovering the digital steps you may already be taking, but didn’t realize
- Seeing how the return on your control investment will bring greater returns on your machines,
your operations and your people - Learning how key tools such as the digital twin of the machine and the Cloud for real-time
data analytics will increase your manufacturing productivity
_____________________________________________________________________________________________
Exploring the new SINUMERIK software release version 4.7 for the SINUMERIK 840D sl and 828D
With such a high technology CNC like the SINUMERIK control, it's critical for us to keep moving its capabilities forward. Large leaps in functionality can be seen with every new software version. With the release of the new SINUMERIK software version 4.7, we have the opportunity to see some of this advancement first-hand.
_____________________________________________________________________________________________
SINUTRAIN — using its fullest potential for SINUMERK 840D sl and SINUMERIK 828D
SINUTRAIN is widely used to demonstrate the full potential of the SINUMERIK CNC. However, we often overlook the fact that it is an extremely powerful, standalone piece of software that has many advanced capabilities. In this webinar, we will explore the full potential of this robust, digital machine control emulator. We will follow the process from installation all the way to customization. Upon completion, attendees will have a much better understanding of how to work with this unique tool.
_____________________________________________________________________________________________