Candleholder
Let there be light!
The Workpiece
"Let there be light!" - bring light into the darkness with the candleholder or simply have a romantic evening together.
The candleholder is made of two parts: the socket as a milled part and the candleholder, which is turned. You can design the socket as you like. Further suggestions are contained in the machining description.
The candleholder can be adapted individually with engravings. A suggestion for lovers can be found at the back.
All information required for production, drawings, tool data and manufacturing description are compiled below.
Note
The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.