Pyramid
Karlsruhe Pyramid
The workpiece
For almost two hundred years a small pyramid has adorned the market place in Karlsruhe and is the last resting place for city founder Margrave Karl Wilhelm. This landmark was the model for an example workpiece in the swiveling course held at the Chamber of Trades and Crafts in Karlsruhe.
The pyramid consists of an aluminum block manufactured on a 3+2 milling machine using swivel cycle CYCLE800.
All information required for production, drawings, tool data and manufacturing description are compiled below.
Note
The programs and files have been created and tested with the greatest care in accordance with the requirements listed in the manufacturing description. However, the manufacturing of the workpieces offered is at your own risk. Siemens accepts no liability for damage to property or personal injury. Workpiece manufacture is only permitted for private and not industrial use. Passing on the manufactured workpieces or production documents to a third party for commercial gain is strictly prohibited.