We're number ONE for CNC machine builders
SINUMERIK ONE digital CNC system
SINUMERIK ONE capitalizes on the advantages that the digital twin brings to machine manufacturers and users. The virtual image becomes the reference variable for real action. Quality and speed in the production of the workpiece also benefit. Read here which results SINUMERIK ONE brings to machine builders.

Siemens Machine Tool Day 2020: Virtual Event on demand
Digitalization in Machine Tool Manufacturing – thinking further
Watch the recorded sessions
Increase the quality & speed of engineering & commissioning
TIA Portal is the central component of a consistently digital engineering process, where the data collected form the basis for the digital twin. The digital twin of automation – the digital image of the control, the machine behavior and the kinematics – offers the ability to virtually test and commission the machine configurations and performance from the TIA Portal.Digital First with SINUMERIK ONE
The digital twin makes a major contribution toward optimizing many types of processes during engineering but also later when the machine is in operation. Combined with the right business model, the digital twin enables machine manufacturers to generate additional business in conjunction with their machine tools.Increased performance for innovative machine tools
SINUMERIK ONE is optimized for performance. Thanks to an innovative system architecture, the system impresses with outstanding productivity. Especially in the field of highly demanding mold making, productivity increases in the double-digit percentage range can be achieved depending on the machine. Innovative software functions tap the potential of the latest processor technologies and enable the parallelization of various processing functions without any loss of performance.
Machine users: you too can discover new ways of thinking
Now that you've seen what SINUMERIK ONE can do for machine builders, learn about the advantages it brings to job shops, tool and mold making as well as for plant managers.