We're number ONE for machine tool users
SINUMERIK ONE digital CNC system
SINUMERIK ONE capitalizes on the advantages that the digital twin brings to machine manufacturers and users. The virtual image becomes the reference variable for real action. Quality and speed in the production of the workpiece also benefit.

Siemens Machine Tool Day 2020: Virtual Event on demand
Digitalization in Machine Tool Manufacturing – thinking further
Watch the recorded sessions
Digital First with SINUMERIK ONE
SINUMERIK ONE enables a consistent “digital first” strategy. This means that key manufacturing processes (e.g. programming, job preparation or process optimization) are always simulated first using digital twins – on detailed virtual images of the controls and machining. The result is faster communication with customers about prices and deadlines, more accurate planning and job preparation and increased productivity, even with falling batch sizes and an increasing range of variants.Improved performance on the shop floor
SINUMERIK ONE is optimized for performance. An innovative system architecture means the system excels with its excellent productivity. In the highly demanding area of mold making, in particular, double-digit productivity gains are a real possibility, depending on the machine. Innovative software functions leverage the potential of the latest processor technologies, so very different processing functions can be run in parallel without performance losses.Ideal for modular as well as compact machines
SINUMERIK ONE is available in several control cabinet-based NCU variants as well as in a compact panel-based PPU (Panel Processing Unit) variant. The PPU version combines the CNC control and a 15'' or 19'' HMI panel in one component. This makes SINUMERIK ONE suitable for both modular and compact machines.

SINUMERIK ONE Media Center
Discover how machine users turn to SINUMERIK ONE to set
new standards in machine tool manufacturing.
EveryONE's a winner

Machine builders: you too can discover new ways of thinking
Now that you've seen what SINUMERIK ONE can do for machine users, learn about the advantages it brings to engineering and commissioning and how the CNC increases the performance of modern machine tools.