Fast Power. Anywhere.

Power to the grid in six months or less. In many areas of the world, the population and economy are developing rapidly – which means that the demand for electrical energy is also increasing at the same pace. With our Fast Power portfolio that is based on standardized configurations, we’re offering  solutions that can provide gas turbine generation capacities in just six months or less.
Would you like to learn more?

Get in touch with us

Tough challenges

Urgently needed power

The availability of electrical power is a major enabler of social and economic development. Some parts of the world are developing so fast that conventional power plant construction would take too long to satisfy the immediate needs. In other cases, the power infrastructure is damaged by natural or man-made disasters, needing fast back-up solutions.
When we look at countries that are on the cusp of development, the demand for electricity very quickly exceeds local supply. Then the task is to develop the infrastructure very quickly.
Tilman Harig, Head of Customer Order Engineering, Power and Gas at Siemens

No time to wait

The construction of a conventional simple cycle gas power plant takes around 12 months. For many fast-developing regions, this is still too long to avoid the risk that power shortages will hinder the march of progress. These areas need new power generation capacities immediately.

Lack of infrastructure

Some regions even lack the infrastructure that would allow the construction of a power plant. These regions not only need a solution for fast power, they also need modular and mobile solutions that only call for minimal infrastructure preconditions.

Temporary need

In other cases, the need for more power is only temporary, for example, the short-term demand in developed regions created by air-conditioning units, or the provision of backup power solutions for emergency relief situations. Mobile power plants are an ideal solution to these needs, as they can easily be relocated to a different site to perform a similar duty after addressing the most immediate need.

An ingenious solution

Fast and reliable electricity deployment

To address the need for fast power, Siemens has developed its Fast Power portfolio. These solutions are designed to provide electricity in six months or less and are tailored to the needs of rapidly developing countries. Our focus is to address diverse customer requirements – from mobile, self-contained units with very fast deployment and installation for the most urgent needs to highly standardized gas turbine packages for both new power plants and quick upgrades of existing plants.

How do I get immediate power to the grid?

Click through our infographic slide show and learn more about Fast Power

Siemens gas turbines for Fast Power solutions

Powerful engines for efficient, reliable and flexible operation

Siemens gas engines for Fast Power solutions

Convincing benefits

Fast, reliable, and economical

Fast Power solutions from Siemens enable feed into the grid in just six months after contract signing. In addition to receiving a power plant very quickly, customers also profit from a reliable, state-of-the-art solution that’s based on proven technology. Our Fast Power solution also delivers an economical power supply. Our mobile and modularized solutions for areas with weak infrastructure reduce the need for expensive and complex preparation work to an absolute minimum.
Our Fast Power solution is an ideal choice for customers in regions with an urgent need for reliable power.
Tilman Harig, Head of Customer Order Engineering, Power and Gas at Siemens

Gas turbines for immediate sale

Another way to address the need for fast power is having gas turbines on stock. Have a look at our gas turbines that are available for immediate sale.

Do you need power quickly?

We have the right solution for your challenge

With over 100 years of experience in power generation, today Siemens is one of the leading companies worldwide for reliable gas turbine solutions. With our new Fast Power portfolio, we can now offer a reliable and economical solution to meet the growing demand for additional short-term generation capacities.

Don’t hesitate to contact us.

Fill out our contact form